- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi, I plan to interface a python 500 Cmos camera with Cypress EZ-USB FX3. The frame rate of the camera is 500 fps(Pixels:600*800). So I'm just wondering to know if it is possible to achieve 500 fps?
Many thanks,
Frank
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Frank,
The GPIF II interface can run at a maximum of 100MHz, with a maximum 32-bit data bus. The maximum throughput supported by the GPIF interface is 32 bits * 100MHz = 3.2Gbps (400MBps).
The data coming from the sensor should be less than or equal to maximum throughput supported by GPIF interface (400MBps) i.e.
600*800*bytes/pixel* 500 < = 400MBps
When GPIF bus width is 32 bits and PCLK is 100 MHz, if Bytes/pixel = 1, then 600*800*1*500 < 400 MBps
Note: 3.2Gbps throughput is for the case when GPIF bus width is 32 bits and 100 MHz clock. At PCLK 100MHz, configuring the GPIF interface for 8/16/24 bits bus width will reduce the data throughput.
Please let me know if any queries on this.
Regards,
Rashi
Rashi