Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
UserP1994
Level 3
Level 3
10 replies posted 10 questions asked 10 sign-ins

Hello,

We want to use CyU3PMipicsiSetSensorControl(CY_U3P_CSI_IO_XRES,CyTrue); in the BootLedBlink example main.c line 83.

We attached also the source code .The result when compile is: 

*** Incremental Build of configuration Debug for project BootLedBlink ****
cs-make all
'Building target: BootLedBlink.elf'
'Invoking: Cross ARM C Linker'
arm-none-eabi-gcc -mcpu=arm926ej-s -marm -mthumb-interwork -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -Wall -g3 -T "C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\/fw_build/boot_fw/cyfx3.ld" -nostartfiles -Xlinker --gc-sections -L"C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\/boot_lib/1_3_3/lib" -L"C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\/fw_lib/1_3_3/fx3_debug" -L"C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\ARM GCC\/lib/gcc/arm-none-eabi/4.8.1" -L"C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\ARM GCC\/arm-none-eabi/lib" -Wl,-Map,"BootLedBlink.map" -Wl,-d -Wl,-elf -Wl,--no-wchar-size-warning -Wl,--entry,Reset_Handler -o "BootLedBlink.elf" ./I2C.o ./cyfx_gcc_startup.o ./main.o -lcyfx3boot -lcyu3mipicsi -lc -lgcc
C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\/fw_lib/1_3_3/fx3_debug\libcyu3mipicsi.a(cyu3mipicsi.o): In function `CyU3PMipicsiRegisterRead':
cyu3mipicsi.c:(i.CyU3PMipicsiRegisterRead+0x54): undefined reference to `CyU3PI2cReceiveBytes'
cyu3mipicsi.c:(i.CyU3PMipicsiRegisterRead+0x68): undefined reference to `_tx_thread_sleep'
C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\/fw_lib/1_3_3/fx3_debug\libcyu3mipicsi.a(cyu3mipicsi.o): In function `CyU3PMipicsiRegisterWrite':
cyu3mipicsi.c:(i.CyU3PMipicsiRegisterWrite+0x50): undefined reference to `CyU3PI2cTransmitBytes'
cyu3mipicsi.c:(i.CyU3PMipicsiRegisterWrite+0x64): undefined reference to `_tx_thread_sleep'
C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\/fw_lib/1_3_3/fx3_debug\libcyu3mipicsi.a(cyu3mipicsi.o): In function `CyU3PMipicsiSetSensorControl':
cyu3mipicsi.c:(i.CyU3PMipicsiSetSensorControl+0xbc): undefined reference to `_tx_thread_sleep'
c:/program files (x86)/cypress/ez-usb fx3 sdk/1.3/arm gcc/bin/../lib/gcc/arm-none-eabi/4.8.1/../../../../arm-none-eabi/bin/ld.exe: BootLedBlink.elf: hidden symbol `CyU3PI2cReceiveBytes' isn't defined
c:/program files (x86)/cypress/ez-usb fx3 sdk/1.3/arm gcc/bin/../lib/gcc/arm-none-eabi/4.8.1/../../../../arm-none-eabi/bin/ld.exe: final link failed: Bad value
collect2.exe: error: ld returned 1 exit status
cs-make: *** [BootLedBlink.elf] Error 1

 

12:55:48 Build Finished (took 2s.213ms)

How can we use this function in bootledblink example?What do we have to include or to configure?

Thanks in advance!

 

 

0 Likes
1 Solution
1 Reply
Rashi_Vatsa
Moderator
Moderator
Moderator
5 likes given 500 solutions authored 1000 replies posted
0 Likes