cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

Keerthy
Moderator
Moderator

 Question: How can I connect multiple image sensors to one CX3 device? Only one image sensor will be active at any point of time.

   


   

Answer:

   

It can be done using the following ways:

   

 

   
1. A high speed analog switch can be used to connect one sensor at a time to CX3. 
https://www.fairchildsemi.com/datasheets/FS/FSA642.pdf

2. A FPGA + Cypress FX3 solution can be used. FPGA should convert the MIPI signal to parallel output. FX3 is can take this parallel data as input and send to the USB host (Refer AN75779). You may use the low cost Lattice MACH XO3L FPGA + FX3 to implement this.

3. Using an ISP with two sensor inputs (this may be an expensive solution). Cypress doesn't have any reference design for the same.
1 Reply
MaLa_302036
New Contributor

 Thanks

0 Likes