- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I'm using cyfxusbi2sdmamode.c example. It configures uart and i2s.
Where this uart is located ?
- Some virtual uart through USB3 cable into my Host ?
- Or it the one exposed by micro usb jtag cable ?
The code says:
/* Configure the IO matrix for the device. On the FX3 DVK board, the COM port
* is connected to the IO(53:56). So since we need to use both I2S and UART,
* configure the GPIF bus to be 32 bit. This does not mean that the GPIF has
* to be in 32 bit configuration, it just means that the whole 32bit shall be
* reserved for the GPIF interface and not available for GPIO. Another option
* is to not use UART, and use I2S_ONLY mode or use an external UART controller
* on the IO(46:49). */
Where is this IO(53:56) ? Can you explain what is IO(53:56) ?
Looking at "SuperSpeed Explorer Kit Schematic.pdf" I can't find IO(53:56).
Solved! Go to Solution.
- Labels:
-
ispn:38621:1:0
-
l1:314:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
UART is used for sending the debug information to the host through a USB 2.0 cable. This is done by making use of a USB-Serial Converter chip as shown in page 8 of the SuperSpeed Explorer Kit Schematic.
IO(53:56) refers to GPIO 53:56 of the FX3 chip. Please find the pin description for FX3 chip at page 15 of the FX3 Datasheet. The link to the same is given below:
https://www.cypress.com/file/140296/download
From this, you can understand that when the GPIF bus width is configured to be 32 bits (as done by this example project), GPIO 53:56 can be used as COM port. If the GPIF data bus width is configured to be 16 bits, then depending on the io_cfg.lppMode, GPIO 53:56 can be used as UART/SPI.
Best Regards,
Jayakrishna
Jayakrishna