cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

LuTr_1679866
New Contributor II

Hello,

   

I successfully managed to send a single bitstream of 160KB on I2C.

   

But the device on the other end is not able to cope with the bitrate, even if my clock is only 100kHz.

   

Is there a way to insert pauses on this bitstream without adding start/stop condition?

   

Is it possible to get the source code for the function CyU3PI2cTransmitBytes?

   

Best regards,

   

Ludovic

0 Likes
1 Reply
Anonymous
Not applicable

You can find the source for this API in the FX3 SDK once you unzip the firmware source in the following location. Please check. 

   

C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\firmware\fx3_sdk_1_3_3_src\fx3_sdk_1_3_3_src\sdk\firmware\src\lpp\cyu3i2c.c

0 Likes