- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
How can we add serial number descriptor to FX3 firmware design? "boot_fw" example firmware has serial number descriptor.
I looked at the example and I added following serial number definition and I called following function in the code but Control Center did not show the serial number. By the way, we can see the bootloader's serial number in Control Center.
Regards,
Ali
const uint8_t CyFxUSBSerialNumDesc [] =
{
0x1A, /* Descriptor size */
CY_U3P_USB_STRING_DESCR, /* Device descriptor type */
'0',0,'0',0,'0',0,'0',0,'0',0,'0',0,
'0',0,'0',0,'0',0,'A',0,'A',0,'A',0,
0,0, /* long word align */
};
apiRetStatus = CyU3PUsbSetDesc(CY_U3P_USB_SET_STRING_DESCR, 3, (uint8_t *)CyFxUSBSerialNumDesc);