- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
- Dears.
My customer is taking into account of usage of FX3S or SD3 to design SD Card Reader.
For my question about the max length of USB3.0, I found https://www.cypress.com/comment/283106.
Do you have any detail benchmark test report or technical description to figure out the performance of FX3s or SD3 as the leghth of usb 3.0 cable
Thank you
Wonjin Han.
Solved! Go to Solution.
- Tags:
- cable length
- fx3s
- sd3
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Wonjin Han,
For A to B type cable, it is 3 m for USB 3.0, and 5 m for USB 2.0.
For compliance tests with B connector fixture, it is a requirement to use 3 m cable.
For the type-C fixture, the maximum cable length is 1.8 meters when testing.
The above cable lengths have been used while testing the cypress USB products (SD3 as well) and that too, with a USB-IF certified cable. If a non-standard cable or a cable with greater length than specified (compared to USB spec), the results may differ as the signal quality is affected.
Other than the above-mentioned cable length (which are recommended by the USB spec), SD3 hasn't been tested further, because the test results will be highly subjective to the application.
If the customer needs to use higher lengths of cable, it is recommended to either use a Retimer or a Hub in between the device and host to maintain signal integrity.
Regards,
Yashwant