cancel
Showing results for 
Search instead for 
Did you mean: 

USB Low-Full-High Speed Peripherals

Anonymous
Not applicable
        Hello! Can anyone help me for my project to build an wireless usb application like wireless webcam. Is CYRF7936 with 4MHz channel bandwidth and 62.5kbps data rate, is it possible to transmit the output of a webcam via wireless.   
I want to ask that, can we use CYRF7936 to make the wireless webcam using wired one? If not then which chip can be used to make it wireless and if yes then, what considerations should be undertaken.   
Thank you   
0 Likes
0 Replies