- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
fx2lp pin 50 is connected to another device.i wanted to generate 2 mili second pulse(active high) from this pin.
so i am using timer for delay genaration.i need 2ms active pulse .how to make pin no 50 initaily low .
fx2lp is operating at 24MHZ,TIMER run at the same rate,
how to put this in code.??
pin 50 at logic low
2ms_delay(); //pin 50 at logic 1 upto 2 mili seconds.
pin 50 at logic low.
regards.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Geethanjali,
Please let know if the mentioned implementation is suitable to your application.
PD5 = 0; // Drive LOW
if(<condition>)
{
PD5 = 1; // Drive HIGH
EZUSB_Delay(2); // Generate 2 ms delay
PD5 = 0; // Drive it LOW
}
Best regards,
Srinath S
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Geethanjali,
I assume that you are using FX2LP in the 56-pin QFN package and the FX2LP is used in either PORTS mode (or) 8-bit slave FIFO mode. Please correct me if I am wrong.
In that case, to drive the pin active HIGH for 2ms, the EZUSB_Delay() function call can be used.
PD5 = 1; // Drive HIGH
EZUSB_Delay(2); // Generate 2 ms delay
PD5 = 0; // Drive it LOW
Please let know if this implementation would suit your application.
Best regards,
Srinath S
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi sir,
you are right,I am using FX2LP in the 56-pin QFN package,FX2LP is used in 8-bit slave FIFO mode.
Pin should be active HIGH for 2ms,after that it should be low and before 2ms high delay,pin should be low.
please see the diagram.
regards,
Geethanjali.
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
Hello Geethanjali,
Please let know if the mentioned implementation is suitable to your application.
PD5 = 0; // Drive LOW
if(<condition>)
{
PD5 = 1; // Drive HIGH
EZUSB_Delay(2); // Generate 2 ms delay
PD5 = 0; // Drive it LOW
}
Best regards,
Srinath S
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello shrinath,
what is that condition?how can i go through this?
regards,
geethanjali.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
The condition will be nothing but when do you want to toggle the GPIO, if you just wish to toggle always irrespective of any condition, then can have it without condition.
For example, I have a requirement where I have to turn on a LED for 2mS when a button is pressed.
In this example I might place the pseudo code might look like as below:
if(button_pressed)
{
Toggle LED which can be achieved may be driving a GPIO
LED_ON;
Delay(2) // 2mS Delay
LED_OFF;
}
Thank you & regards,
Sudheer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I have written above code in my firmwre with OED=0x20;,but i cant see pulse at this pin when i probe with oscilloscope.
did i miss anything?is it any register or configuration is there to make pin as output or input?
regards,
geetha.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Geetha,
- The OEx register of the corresponding port to which the used GPIO belongs must be set such that the pin is configured as an output.
- For example, in case you are using PA1 as output, the following line would configure the pin.
OEA = 0x02;
Best regards,
Srinath S
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello shrinath,
I have used OED=0x20; for PD5 port.but i dint get the pulse on this pin.
regards,
geetha.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Geetha,
- Please check if you have used the IOD |= 0x20 and IOD |= 0x00 statements after you have configured the pin using the OED = 0x20 statement.
- OEA register setting only configures the pin as an output pin. IOA register has to be written with the value to drive the pin either HIGH or LOW.
Best regards,
Srinath S
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello shrinath,
PD.5=0; ->This statement is not enough to drive the pin to low?
are you saying that to replace PD.5=0 to IOD=0x20?
regards,
geetha.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Geetha,
- PD5 = 0 or PD5 = 1 can also be used to drive the pin. Please let me know if you are using it this way.
- Please share the code snippet and also the waveform captured on this pin.
Best regards,
Srinath S
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
void TD_Init( void )
{
CPUCS = 0x02; /// CLKSPD[1:0]=01, for 24MHz operation, output CLKOUT
PINFLAGSAB = 0x08; // FLAGA - EP2EF
SYNCDELAY;
PINFLAGSCD = 0xE0; // FLAGD - EP6FF
SYNCDELAY;
OED=0x20; //ENABLE PD.5
// IOD=0x20;
EZUSB_InitI2C();
IFCONFIG = 0x03; // external clock, synchronous, Slave FIFO interface,OE disabled.
SYNCDELAY;
// EP4 and EP8 are not used in this implementation...
EP2CFG = 0xE2; //in 512 bytes, 4x, bulk
SYNCDELAY;
EP6CFG = 0xE0; //in 512 bytes, 4x, bulk
SYNCDELAY;
EP4CFG = 0xA2; //out 512 bytes.4x,bulk
SYNCDELAY;
EP8CFG = 0x02; //clear valid bit(not used)
SYNCDELAY;
FIFORESET = 0x80; // activate NAK-ALL to avoid race conditions
SYNCDELAY; // see TRM section 15.14
FIFORESET = 0x02; // reset, FIFO 2
SYNCDELAY; //
FIFORESET = 0x04; // reset, FIFO 4
SYNCDELAY; //
FIFORESET = 0x06; // reset, FIFO 6
SYNCDELAY; //
FIFORESET = 0x08; // reset, FIFO 8
SYNCDELAY; //
FIFORESET = 0x00; // deactivate NAK-ALL
FIFOPINPOLAR = 0x04; // Setting SLWR active HIGH
SYNCDELAY;
EP6FIFOCFG = 0x00;
// EP6FIFOCFG = 0x08;
SYNCDELAY;
EP6AUTOINLENH = 0x02;
SYNCDELAY;
EP6AUTOINLENL = 0x00;
SYNCDELAY;
PORTACFG = 0x02;
TCON |= 0x04;
IE |= 0x84;
PX1 = 1;
EZUSB_WriteI2C(Image_Sensor, 0x03, REG012);
EZUSB_WriteI2C(Image_Sensor, 0x01, REG014);
}
void TD_Poll( void )
{
PD5 = 1; // Drive HIGH
EZUSB_Delay(100); // Generate 100 ms delay
PD5= 0; // Drive it LOW
//SYNCDELAY;
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello shrinath,
anything wrong with the above code snippet?
regards,
geetha.
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
Hello shrinath,
1)Its enumearting properly,i am able to recieve proper data in IN bulk ENDPOINT.
2)PD5 pin is connected to one of the pin of image sensor,its directly connected to image sensor(without any pullup/pulldown resistor,series register).
regards,
geetha.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Geetha,
Please let me know how do you identify the pin is not toggling. In case you are probing the lines, kindly, share the screenshot.
Best regards,
Srinath S
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello shrinath,
yes,i am probing the pin PD5 and checking the same with oscilloscope.
its not toggling,just showing single line.
regards,
geetha.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello shrinath,
I am getting this warning message,is it because of this?but its build with 0 errors and 0 warnings.
and i2c read and write function works as expected.
regards,
geetha.
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
Hello shrinath,
please share the .hex file.
regards,
geetha.
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
Hello shrinath,
I probe the PD5 pin,its not togling?I am getting no signal found in cro.
regards,
geetha.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Geetha,
I tested this firmware on the FX2LP DVK and I could see the toggling on PD5 pin which I had shared as a screenshot. So, this seems like an hardware issue on your board. Kindly, recheck your onboard connections and ensure you are probing it properly.
Best regards,
Srinath S
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello shrinath,
If i set IFCONFIG=0x03; i.e.slavefifo configuration,led is not blinking.
if i comment IFCONFIG=0x03; i.e. default port mode,led is blinking.
can't i use FD[8:15] or PD[0:7] pins as GPIO when its in slavefifo configuration with 8 bit data bus(WORDWIDE=0).
regards,
geetha.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello shrinath,
PD3 pin is connected to led.
if i use this below code,led is blinking with bulkloop.c example project.
TD_Init()
{
OED=0x08;
IO=0x08;
}
If i use above code in slave.c slavefifo configuration,led is not blinking.
I have set EP6FIFOCFG=0x00; //WORDWIDE=0;
Why this is happening?
regards,
geetha.