Anonymous
Not applicable
Oct 12, 2009
05:40 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Oct 12, 2009
05:40 AM
Hi
I written the firmware using keil software.and converted into .hex to.iic using hextobix.exe.
now i have some confusion that is
I want store my firmware that is firmware.iic in to the EEPROM which is connected via I2C to cy7c68013a, and load the firmware into cy7c68013a from EEPROM when i power-up the board.
1)How can i download the firmware into EEPROM first time i.e using cyconsole tool.before downing the firmware.iic file into the EEPROM i have to be load any file into the cy7c68013a (i.e. Vend_Ax.hex ) or only Firmware.iic file is enough
2)CYUSB.sys file detect the hardware and enumerate or i have to write any driver at host side to detection and enumeration the device i.e cy7c68013a
I written the firmware using keil software.and converted into .hex to.iic using hextobix.exe.
now i have some confusion that is
I want store my firmware that is firmware.iic in to the EEPROM which is connected via I2C to cy7c68013a, and load the firmware into cy7c68013a from EEPROM when i power-up the board.
1)How can i download the firmware into EEPROM first time i.e using cyconsole tool.before downing the firmware.iic file into the EEPROM i have to be load any file into the cy7c68013a (i.e. Vend_Ax.hex ) or only Firmware.iic file is enough
2)CYUSB.sys file detect the hardware and enumerate or i have to write any driver at host side to detection and enumeration the device i.e cy7c68013a
1 Reply