cy7C68013 C0.C2 mode

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

 i have write a  firmware, and use the kneil 4 to compile it, when output, i use the command as below:

   

   

Hex2bix.exe -i  -o bulktogpif.iic bulktogpif.hex -f 0xC2 -v 0x0451 -p 0x32AF

   
    the i use the control center download it to EEPROM, and the software show it programmed successfully, and i also load    
   
    the sprit file and display the sprit,   
   
        
   
    But, it seems that the usb is started as the C0 mode,    
   
        
   
    can you help me, how can i know whether EEPROM is programming successfully and the 68013 is working by load the firmware which is written by myself?   
0 Likes
1 Reply
Anonymous
Not applicable

 Hi ,

   

Please share the .*iic file which you have used to program the EEPROM. you can read the contents of EEPROM by using some vendor commands. Refer vend_ax example avaialble in the path (C:\Cypress\USB\CY3684_EZ-USB_FX2LP_DVK\1.0\Firmware)after installing CY3684. Also refer the application note in the following link      http://www.cypress.com/?docID=41632.

   

if possible share the firmware also.

   

 

   

Regards,

   

Vikas.

0 Likes