Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB low-full-high speed peripherals Forum Discussions

sarah
USB low-full-high speed peripherals
Dear Sir/Madam,   GreenSoft Technology, a leading provider of environmental compliance data management services and software for the global electronic... Show More
Ciple
USB low-full-high speed peripherals
My system have a EZ-USB FX2LP. In "Receiver sensitivity Test", my system is failed. "Pass Limits:<= 200.000 mVDevice receiver sensitivity [218] (Worst... Show More
Mitchell_shen
USB low-full-high speed peripherals
We are use CY7C65211 as USB to I2C bridge.(VID_04B4 & PID_0004) But CYUSB3 driver test fail of DFX support. Does Cypress have new CYUSB3 driver to su... Show More
BrWu_4382966
USB low-full-high speed peripherals
I have a custom board based on the FX3S processor with an attached debugger section using the CY7C65215. The connections of the CY7C65215 are a direct... Show More
hjh
USB low-full-high speed peripherals
Hi I am a developer looking at Cy7c68013 as a replacement for cy7c68001. When using the Cy7C68001 Device, "BUSACTIVITY interrupt : detected either an ... Show More
CL
USB low-full-high speed peripherals
Hi, I met the problem when trying to update firmware to a new EEPROM in FX2LP in Windows 10/ 64-bit. The device can't be identified successfully and t... Show More
JakobVollmer
USB low-full-high speed peripherals
Hello everybody, I have a project with my team for which we want to use the CYUSBS234 USB-SPI-Bridge. Unfortunately I only found one C ++ library for... Show More
kita_4790911
USB low-full-high speed peripherals
Hi, I'm using cy3684 DVK , the windows version is 7 and 10(2 computers) working on Korean version,   The problem is example An66806 hex file does not ... Show More
NoAr_1540581
USB low-full-high speed peripherals
Hello Is there a file that can simulate the waveform of the HX2VL downstream port?   Is the IBIS model below a model that c... Show More
kita_4790911
USB low-full-high speed peripherals
I'm using CY3684 Development Kit, using windows 10 64bit user.   I'm having problem with an66806, the hex file that I can download does not load on th... Show More
Forum Information

USB low-full-high speed peripherals

Discussion forum regarding USB low-full-high speed peripherals topics.