Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB low-full-high speed peripherals Forum Discussions

rossi
USB low-full-high speed peripherals
I'm working on to develop usb 2.0 host firmware which can handle USB camera(UVC). The device(WebCam) provides video data through isochronous endpoint.... Show More
ksg03034
USB low-full-high speed peripherals
I have a CY7C68013A-based design that I am supporting. The design uses the GPIF to interface with an FPGA. We are using the IFCLK in internal mode (48... Show More
Yosuf
USB low-full-high speed peripherals
We have a CY7C68013 FX2LP processor connected to an FPGA device.  Data is received from a host processor via Full Speed USB on EP2.  Since it is FS US... Show More
marcus
USB low-full-high speed peripherals
Hi,I've a problem  with a special laptop and my cy7c68013A device (driver version 3.4.7).After booting the Laptop my device is running fine (I can com... Show More
yakgg
USB low-full-high speed peripherals
HI, I use USB Control Center to wite to EEPROM as shown in Figure 7-17 in CY3674/CY3684 EZ-USB Development Kit User Guide. But I found I can not write... Show More
brant123
USB low-full-high speed peripherals
I met a following error on FX2LP-cy7c68013a. The project is designed as USB2.0 HS mode. When Host sent NYET PID,  USB PHY has no any answer, sound car... Show More
vishwasd19
USB low-full-high speed peripherals
Hello, I am using an electroencephalogram (EEG) that uses a CyUSB.sys driver. I am looking to get the incoming EEG data into MATLAB.  I am not a coder... Show More
PaRi_1293246
USB low-full-high speed peripherals
Hello, I need to buy a compiler for the FX2LP18 USB microcontroller CY7C68053.  Can you confirm that the Keil PK51 is compatible with the CY7C68053? T... Show More
azot_0
USB low-full-high speed peripherals
Hi,what is the maximum chunk size for BULK/Interrupt transfer from the host to the slave for both FX2/USB2 or FX3/USB3 using libusb or cypress driver?... Show More
Wanjie
USB low-full-high speed peripherals
We used this CY7C65630-56LFXA chip on our equipment. On each unit, we have two chips to control 6 SD cards. While on Win7 OS, we have no problems to h... Show More
Forum Information

USB low-full-high speed peripherals

Discussion forum regarding USB low-full-high speed peripherals topics.