USB Low-Full-High Speed Peripherals

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
Jobin
USB Low-Full-High Speed Peripherals
For our new application, we are trying to stream data in & out over EP02 and EP86 eps of CY7C68013A128AXC. We are using VC++ host app to source/sink t... Show More
Edmond
USB Low-Full-High Speed Peripherals
Hello. I purchased the CYUSBS236 kit. I'm trying to read/write my target slave device thru SPI using the tool. Only utility provided with the tool is ... Show More
Anonymous
USB Low-Full-High Speed Peripherals
Looking for a device which is able to work with 5V power supply and the CY7C65211 seems to meet this requirement. But in the dataheet is mentioned tha... Show More
Shaunie85
USB Low-Full-High Speed Peripherals
Hey to all, I have a problem with my RS485 TX EN signal. The TX_EN Signal does not have a fixed length. That means after the message the signal does n... Show More
lee
USB Low-Full-High Speed Peripherals
Hi, I got the same problem. "Why in manual mode the slave fifo interface flags don't change?"  and I can not get the answer from this case. It has bee... Show More
Anonymous
USB Low-Full-High Speed Peripherals
Hi,We are using CY7C68034-56LTXI on our design to access 2GB NAND Flash part# MT29F16G08AJADAWP. Please can anyone clarify me on following points.1. W... Show More
Anonymous
USB Low-Full-High Speed Peripherals
Hello,    Can you tell me if there is a driver WIN10 for device cy7c68001         Best regards         Alain Show More
EfMi_2218266
USB Low-Full-High Speed Peripherals
Hello, We are using CY7C65215-32LTX in our board as USB2UART bridge, we are using SCB0 only (to get 3M baud) and we face two issues:a) We configured t... Show More
MuPa_4609196
USB Low-Full-High Speed Peripherals
Dear Sir,We are using CY7C65213 In USB Power,The Board is working fine, But at random cases, it fails on the long run(Once in 24hrs)Once the board is ... Show More
Anonymous
USB Low-Full-High Speed Peripherals
Hello everybody,    i have a CY7C65213-32LTXI chip on my custom board.    It should work as a UART interface,    but when i connect to it it says it i... Show More