USB low-full-high speed peripherals Forum Discussions
I have got a FX3S RAID-on-Chip USB Dongle and I'm using FT232H from adafruit to debug via UART but I don't know why debug messages doesn't appear on TeraTerm I also tried displaying using Putty but still didn't work. I did the following:
1- I installed necessary uart to usb bridge adafruit driver and did a loopback test and it worked.
2- I double checked the connections between the RAID-on-Chip USB Dongle and adafruit UART to usb converter(Tx, Rx and gnd) and they are ok.
3- I used the following setting to display debug messages using TerraTerm (baud rate 115200, 1 stop bit, Data 8 bit, no stop bit, no flow control)
But debug messages never displayed!
Any helpful reply would be appreciated
Show LessA few months ago I requested to start a Re-selling process for the CyUsb3.sys (see Re: Current USB- Driver for CY7C68013 ). Cypress Support opened me the Case: 00474167. Unfortunately, I had some issues with the Microsoft Hardware Dashboard Account and thus we closed the support case. I finally could solve the problems with the Microsoft hardware dashboard account and would like to re-open the support case. If that is not possible i would like to open a new case for starting the driver resell procedure.
Regards
Yves
Show LessHello,
I have interfaced fx2lp with image sensor,it is working fine.now i need to increase exposure by using SET command from GUI,
what are the changes need to modified in firmware? is there any condition? if you have any sample code related to this please do share me.
Thanks ®ards
Bhavya
Show LessHello,
Following the firmware example for the OV5640 provided with the Cypress EZ USB Suite I have been able to produce working firmware for my camera board. When connected to a smart phone (have tried Google Pixel, Galaxy A5 and Galaxy S8) I get a steady stream of 640 X 480 @ 30fps.
When I connect the camera module to a Dragonboard 410C which is running Android, I use the same application but I get no stream.
By changing the DMA buffer to 8FC0 (+12 header, +4 Footer) and DMA Count to 3 I have been successful in getting some complete images but it is very inconsistent.
I also found that it helped stability of the stream to remove the while loop from the 'Produce event' in the DMA Callback function, however, the stream is still far from serviceable.
I am happy to provide extra information about setup if required.
Any idea what is going on?
*EDIT* - I have successfully streamed to the same Dragonboard using the same firmware when Ubuntu Core 18 (ish!) was installed on the device.
Show LessI'm having problems getting this working and I'm wondering if there is a working example with this configuration?
Ultimately I am trying to put together an application with two CDC USB ports (a CDC to UART bridge and debug port) and a GPIF II USB interface all under one configuration.
Show Less@
I have send signal from xilinx spartan 6 xc6lx9 to pc via cyc768013-56pvcx usb in slave fifo mode, i need help in measuring frequency of sent signal via labview>
Any Help?.
Show LessIs there any documentation that exposes the details of the virtual com port protocol for the CY7C65215 device.
I'm trying to avoid using the provided libraries and roll my own.
Show LessHi
We would like to implement a RNDIS application on your CY7C68013A and have found that all Application Notes are obsolete
Where can we find the necessary sources for such an application ? How we can proceed ? Are there other known existing solutions?
Thanks
Show Less