cancel
Showing results for 
Search instead for 
Did you mean: 

USB Low-Full-High Speed Peripherals

Anonymous
Not applicable

 Hi

   

What am i do configuration for i2c setting in slave fifo mode?

   

 

   

Now i use 56pin fx2lp and 16bitdata slave fifo. 

   

So i have not enough pin. 

   

Could you please let me know what configuration need to me?

0 Likes
1 Reply
Anonymous
Not applicable

Hi dv2,

   

Eventhough you are using 16-bit slave FIFO interface you have the I2C hardware block (SDA and SCL lines) to talk to I2C device.

   

SDA and SCL lines are seperate from the slave FIFO interface. So you should be able to use 16-bit slave FIFO and I2C lines at the same time.

   

Thanks,

   

sai krishna.

0 Likes