Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
gean_3054931
Level 5
Level 5
10 likes given 5 likes given First like received

Hello,

is keil2 (fx2lp ide)supports release mode (release version build)and debug mode congiguration settings?

thank you.

geetha.

0 Likes
1 Solution
SudheerG_41
Employee
Employee
5 sign-ins Welcome! 25 comments on KBA

Hi Geethanjali,

Looks uVision doesn't support this type of Build Configurations.

Please see the following URL : Debug/release configuration

This should help you in achieving Debug / Release configurations.

The target options needs to be customized for different targets to achieve this.

Thank You & Regards,

sudheer

View solution in original post

7 Replies
Sananya_14
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hello Geetha,

In Keil, you dont have separate modes for Debug and Release. You can have the .hex file generated in case of Debugging also, by choosing the option under Output tab in Target options.

Best Regards,

Sananya

0 Likes
SudheerG_41
Employee
Employee
5 sign-ins Welcome! 25 comments on KBA

Hi Geethanjali,

Looks uVision doesn't support this type of Build Configurations.

Please see the following URL : Debug/release configuration

This should help you in achieving Debug / Release configurations.

The target options needs to be customized for different targets to achieve this.

Thank You & Regards,

sudheer

Hello,

the target options needs to be customized for different targets to achieve this.

-->

can you please tell me how to set target options?

thank you.

0 Likes

Hello Geetha,

Right click on the target name in the project window and choose 'Options for Target <TargetName>'.

Best regards,

Srinath S

0 Likes

Hi Geethanjali,

Once you created a new target, each target has its own option tab as shown below.

You have to go to each available tab and whatever options you would like to enable you can activate for that particular target.

For example in C51 tab there under Code Optimization uV2 has two options, one is Favor Speed and other is Favor size.

So, for one of the target you can use this option as Favor Speed and for other target you can use this options as Favor Speed.

pastedImage_1.png

Regards,

Sudheer

Hello sir,

Like in fx3 sdk.there is a option for selecting debug and release version mode build.is there anything same in the keiluvision2 ?

what you are saying is for code optimisation,please tell me clearly.

thanks

geethanjali.

0 Likes

Hi Geethanjali,

uV2 itself doesn't have this feature as discussed in the following URL:Debug/release configuration.

Thank You & Regards,

Sudheer