cancel
Showing results for 
Search instead for 
Did you mean: 

USB Low-Full-High Speed Peripherals

Anonymous
Not applicable

I am having a cmos camera with 8 bit parallel output. Can anybody suggest me a USB controller which can be used to convert the 8 bit parallel data to USB 2.0 standard data.

   

I am working on embedded linux OS based on ARM9 based processor. 

   

Thank You

   

GIGIN

0 Likes
3 Replies
Anonymous
Not applicable

Hi,

   

         EZ-USB® FX2LP™ (CY7C68013A/14/15/16A) is best suited for your application . Please see http://www.cypress.com/?id=193 and http://www.cypress.com/?rID=57610 for more information.

   

Thanks 

   

Prajith

0 Likes
Anonymous
Not applicable

 Hi Prajith, 

   

Thanks for the reply . 

   

Could you please guide me where to purchase the evaluation board ? Do you have any  demo application for 8bit cmos camera interface ? 

   

 

   

Thank You

0 Likes
Anonymous
Not applicable

Please create a tech support case (MyAccount -> MyCases) so that one of your engineers can you guide you with the same.

   

Regards,

   

Anand

0 Likes