USB Hosts Hubs Transceivers

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
Augustine_Yeh
USB Hosts Hubs Transceivers

Hi Cypress

We need CYUSB3314 firmware( bin file) for disabled U1 and U2 , Can you provide it to us, Thank !!

 

bodangly
USB Hosts Hubs Transceivers
I have the above schematic implemented. I changed the MODE_SEL resistors to put it into internal rom configuration. However, it is stuck with the sus... Show More
TeMa_2997106
USB Hosts Hubs Transceivers
Is it possible to use an crystal oscillator instead of crystal unit as the clock input for the HX3? If it is possible, my understanding is that the os... Show More
HCJung
USB Hosts Hubs Transceivers
Hello,  I have a question about the external X-tal load capacitance for CY7C65631-56LTXI USB hub. I have one or two downstream(thermal cam module or I... Show More
can2021
USB Hosts Hubs Transceivers
I would like to notify external logic when the CYUSB4357 Hub detects when the upstream USB3 link is in suspend.  Can firmware assign a GPIO to signal ... Show More
GrCa_1363456
USB Hosts Hubs Transceivers
How can I replace an HX2VL, CY7C65632-28LTXC, with a HX3, CYUSB2304-68LTXI? Is it possible to set PID or Maximum Power in ROM on HX3? Configuration of... Show More
NoAr_1540581
USB Hosts Hubs Transceivers
Hello I am understanding  that unused pins can be left unconnected.But , please let me know if there is any problem in the following cases. Q1)  If PO... Show More
can2021
USB Hosts Hubs Transceivers
Does the CYUSB4357 Hub support Selective Suspend between the USB2 and USB3 channels?  That is, are the active and suspend states of both USB2 and USB3... Show More
NoAr_1540581
USB Hosts Hubs Transceivers
Hello When using with SELFPOWER (ExternalPower), as shown in the figure of the data sheet, there is a description that the VCC pin is N.C.  Q) But, pl... Show More
itayc
USB Hosts Hubs Transceivers

Hi,

Where can I get an OrCAD symbol and foot print for the CYUSB3304-BVXC?

Thanks,

Itay

Board Information

USB Hosts Hubs Transceivers

Discussion forum regarding USB Hosts Hubs and Transceivers topics.
Top liked authors