- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Good morning everyone,
I'm trying to develop a small board using a 2-ports HUB CY7C65634-48AXC.
At the moment there are no downstream devices connected to the HUB ports, i'm just focusing on getting the HUB device itself up and running.
As a clock source I'm using a programmable oscillator set to 12 Mhz; clock source selection inputs of the Hub IC (SEL48/ SEL27) are connected according to the datasheet specs (both input pulled up to logic "1").
What I see is the following: when I try to plug the board into a windows PC, the device is not enumerated and recognized:
"The last USB device you connected to this computer malfunctioned, and Windows does not recognize it."
If I look at the board with a scope:
- Power rails are OK;
- When I plug USB into the PC, some transactions are visible on D+/ D- USB lines for about 2/3 seconds;
- Something strange happens on the CLK line: after 2/ 3 seconds from the startup, the signal amplitude gets lowered (around 2.8 V instead of 3.3 V); also, if I check the XOUT pin on the Hub IC, I can see a 12 MHz signal at the very beginning, but with a "slow" rising slope,then the signal get become a continuos 3.3 V.
Do you have any hint on what I can check in order to isolate the issue? I've already double checked the schematic and everything seems fine and according to the Datasheet requirements.
Thanks in advance,
Regards,
Fabio