- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I have a few questions about CY7C65631 chip.
I need a high-speed 4-port USB hub chip to connect to raspberry pi unit.
My first question is about compatibility with Linux. I am kind of nervous about compatibility issues. Is there any compatibility issue between CY7C65631 and linux?
Secondly, I am kind of confused about programming eeprom connected to CY7C65631. How is it actually programmed? Do I have to pre-program before soldering the EEPROM or is it programmed through the hub via USB? Is it OK to completely omit the EEPROM? If you can provide me with any compatible EEPROM manufacturer number I would appreciate it.
Lastly, I'd like to know if I can use an oscillator to run the chip instead of crystal. What should be the voltage level of the oscillator? There aren't any guidelines about the clock pins.
Thanks in advance.
Solved! Go to Solution.
- Labels:
-
USB Hosts Hubs Transceivers
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
HX2LP can work on a Linux host since it needs standard hub class drivers which are present with Linux.
The EEPROM doesnt have to be pre-programmed as HX2LP is capable of programming the EEPROM using Blaster utility. You could also eliminate the EEPROM since it has a ROM with default configuration that it can use for boot-up. However, please ensure that the SPI data line has the required pull-down resistor even when not connected. Please refer to 25LC040 which is used in the HX2LP CY4606 DVK.
Yes, an oscillator can also be used instead of the crystal. You can refer to the App Note for clock requirements-https://www.cypress.com/documentation/application-notes-obsolete/an49150-schematic-and-layout-review-checkli...
Best Regards,
Sananya
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
HX2LP can work on a Linux host since it needs standard hub class drivers which are present with Linux.
The EEPROM doesnt have to be pre-programmed as HX2LP is capable of programming the EEPROM using Blaster utility. You could also eliminate the EEPROM since it has a ROM with default configuration that it can use for boot-up. However, please ensure that the SPI data line has the required pull-down resistor even when not connected. Please refer to 25LC040 which is used in the HX2LP CY4606 DVK.
Yes, an oscillator can also be used instead of the crystal. You can refer to the App Note for clock requirements-https://www.cypress.com/documentation/application-notes-obsolete/an49150-schematic-and-layout-review-checkli...
Best Regards,
Sananya
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks for the response.