cancel
Showing results for 
Search instead for 
Did you mean: 

USB Hosts Hubs Transceivers

NaMo_1534561
Contributor II

Hello,

When using the HX3 with an external clock, please tell me the specifications of the VIH and VIL of the clock signal.

Best Regards,

Naoaki Morimoto

0 Likes
1 Solution
Anonymous
Not applicable

Hi Morimoto-san,

The supply voltage of the oscillator should be 1.2V for HX3 to work with.

Please use the oscillator with supply voltage of 1.2V or lesser.

Regards,

Anil

View solution in original post

0 Likes
9 Replies
YangyangC_06
Employee

Hi Naoaki,

Please check the screenshot below.

BaiduShurufa_2017-10-17_17-48-16.bmp

0 Likes
NaMo_1534561
Contributor II

Hello,

I think that "Amplitude" is the distance between the top and the bottom of waveform.

What I would like to know is the voltage of min and max of the signal input to HX3.

Best Regards,

Naoaki Morimoto

0 Likes
YangyangC_06
Employee

Hi Naoaki,

You can find the information in the datasheet of HX3.

BaiduShurufa_2017-10-18_9-17-51.bmp

0 Likes
NaMo_1534561
Contributor II

Hello yyca,

Thank you for your reply. But I am confused with your answer.

If VIH and VIL follow the definition in  DC specification of Table8,

  VDD_IO : 3.0V to 3.6V

  VIH_max = VDD_IO = 3.6V

  VIH_min = 0V

So, amplitude is 3.6 - 0 = 3.6V

It violates the specifications in Table6.

(Table6 seems to copy the specification of 1.2V core supply as it is.)

Please check the specifications of the external clock that can be connected to the HX3 once again.

Best regards,

Naoaki Morimoto

0 Likes
YangyangC_06
Employee

Hi Naoaki Morimoto,

The oscilator and IO block are two different things. There is no relationship between them

If you want to know VIN and VIH of IO block, refer to table 8.

If you want to know the requirment of external clock, refer to table 6.

0 Likes
NaMo_1534561
Contributor II

Hello yyca,

How about the VIN and VIH for external clock input signal? Table6 doesn't have it.

I will change my question.
What is the part number of the clock oscillator recommended by Cypress as the external clock of the HX3?

I will refer to that oscillator datasheet.

Best Regards,

Naoaki Morimoto

0 Likes
YangyangC_06
Employee

Hi Naoaki Morimoto,

We don't have the recommended oscillator for HX3.

You could choose any oscillator which fits in the requirement in table 6.

0 Likes
NaMo_1534561
Contributor II

Hello yyca,

Can I use this oscillator?

SG-210SCB

http://www.mouser.com/ds/2/137/G-210SCB_en-1003249.pdf

Regards,

Naoaki Morimoto

0 Likes
Anonymous
Not applicable

Hi Morimoto-san,

The supply voltage of the oscillator should be 1.2V for HX3 to work with.

Please use the oscillator with supply voltage of 1.2V or lesser.

Regards,

Anil

View solution in original post

0 Likes