- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
While I was trying to configure the CY4541 EVK as a CCG4 Monitor I encountered the problem that I cant program the firmware onto the CYPD4425. Trying to do so gave the following error: "Error: Configuration table version is not compatible with device firmware".
The config table major version for a CCG4 monitor is locked to version 2 in the EZ-PD configuration utility. The base version of the CYPD4225 firmware is 1.0.0.263.
Is there a way to update the base version of the CYPD4225 to version 2 or higher? I tried to look for a way to do so myself but couldn't find a solution.
Thank you in advance!
Solved! Go to Solution.
- Labels:
-
ispn:39572:1:0
-
l1:314:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
CYPD4225 can be used for the Monitor application, however as I have stated earlier, CY4541 has Notebook firmware by default which is expecting Config table major version 1. You need to use the actual "Monitor" application firmware which is available in Dock SDK. But this firmware may not be directly compatible with the EVK. You have to check pin compatibility and then program.
Pranava
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
"Monitor" configuration in the Configuration utility is for the Dock design. The firmware for the same can be found in EZ-PD Dock SDK.
CY4541 will by default have Notebook firmware running, therefore "Notebook" configuration should be used with that. This configuration will have option to change Config table major revision to 1.
Pranava
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Pranava,
Thank you for your reply!
I found that using the "Notebook" configuration is capable with the CY4541. I however want to change it to a "Monitor" configuration so i can check how certain pins behave.
In the configuration tool it is possible to select the CYPD4225 with the "Monitor" configuration. Is it simply not possible to change the config major table version on the CY4541 EVK? If so could you explain why the CYPD4225 is listed with the "Monitor" configuration but cant be used?
Thank you in advance!
Best regards,
hbCIN
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
CYPD4225 can be used for the Monitor application, however as I have stated earlier, CY4541 has Notebook firmware by default which is expecting Config table major version 1. You need to use the actual "Monitor" application firmware which is available in Dock SDK. But this firmware may not be directly compatible with the EVK. You have to check pin compatibility and then program.
Pranava