Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

roprc_3346246
Level 2
Level 2

at the source side we have a tusb1046 switch/retimer and a ccg3 .

At the sink side (a viewfinder) we only have a ccg3.

we use display port alternate mode.

our question is if we also need a switch at the sink side??

thanks

Ron

1 Solution

Hi Ron,

1. If you are using type-C receptacle and plug combination you will not need a switch. If you have both USB-C connectors as receptacles, connected via a type-C cable (EMCA) then you will require a switch.

DP source (FPGA) <---->Switch<------> USB-C receptacle <---------------------> USB-C plug <------> DP sink (FPGA)

otherwise,

DP source (FPGA) <-----> Switch <-----> USB-C receptacle <---------- USB-C cable ----------> USB-C receptacle <-----> Switch <-----> DP sink (FPGA)

2. CCG will detect the C-connector reversal and control the switch. If other than 4-Lane DP is used and other modes are used, it will need switch at both sides. This will be negotiated over CC lines. The connector reversal and CC orientation detect is a part of the type-C specification from USB-IF.

Regards,

Rajath

View solution in original post

0 Likes
3 Replies
RajathB_01
Moderator
Moderator
Moderator
250 replies posted 100 replies posted 50 replies posted

Hi Ron,

If you require USB3.0 communication at the sink side also, you will require a switch at the sink (for example: https://www.paradetech.com/products/ps8742/​ ). If you don't require USB, you can directly route the data lanes from type-C to DP sink with only CCG3 (for example refer CCG3 C-DP dongle application in CCG3 datasheet).

Regards,

Rajath

0 Likes

Hello Rajath,

Thanks for your answer.

Its a bit confusing to me.

The situation is as follows:

-a broadcast camera(source) with FPGA with displayport core(transmit), TUSB1046 switch/retimer, CCG3, USB-C connector.

-a vieffinder(sink) with USB-C connector, CCG3 and FPGA with displayport core(receive) (4 DP signal lanes directly connected to FPGA).

We only use USB 2.0 and not USB3.0/3.1!

Questions:

1-Do we need a switch at the viewfinder side to control the C-type connector reversal?

2-where can i find documentation about this C-connector reversal protocol?

is there any handshaking about this via the CC lines or does switching happen autonomous on eac side (source--sink)?

Thanks in advance.

Ron Proveniers

0 Likes

Hi Ron,

1. If you are using type-C receptacle and plug combination you will not need a switch. If you have both USB-C connectors as receptacles, connected via a type-C cable (EMCA) then you will require a switch.

DP source (FPGA) <---->Switch<------> USB-C receptacle <---------------------> USB-C plug <------> DP sink (FPGA)

otherwise,

DP source (FPGA) <-----> Switch <-----> USB-C receptacle <---------- USB-C cable ----------> USB-C receptacle <-----> Switch <-----> DP sink (FPGA)

2. CCG will detect the C-connector reversal and control the switch. If other than 4-Lane DP is used and other modes are used, it will need switch at both sides. This will be negotiated over CC lines. The connector reversal and CC orientation detect is a part of the type-C specification from USB-IF.

Regards,

Rajath

0 Likes