Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB EZ-PD™ Type-C Forum Discussions

Sort by:
jpm-janz
USB EZ-PD™ Type-C
Hello Infineon community. Im currently working on a project with a TUSB1046 instead of a PS8740. Changing the device adress and some registers worked ... Show More
beewoo
USB EZ-PD™ Type-C
Hi,  I am using the CYPD3120 in a custom USB-C receptacle to DP sink design (4x DP1.4 lanes). This board will have an external MCU onboard, and given ... Show More
osmayto
USB EZ-PD™ Type-C
I am drawing the architecture of our new system and have some questions about it: 1)Normally left board has 20V fixed supply and will provide 20V thr... Show More
Ivan_Lee
USB EZ-PD™ Type-C
  Dose Host SDK 3.6 support Intel meteor lake? Which config folder is used for intel meteor lake?   Show More
gcons
USB EZ-PD™ Type-C
Hello  I am using CYPD3177 in my design. The issue is when I set Vmin/Vmax to 20V and the negotiation is completed there is a huge inrush current afte... Show More
AhKh_4675286
USB EZ-PD™ Type-C
Hi, I have placed the CYPD3176 on a PCB and I would like to configure it with EZ-PD and program it with PSoC Programmer. Can you provide a hex file pl... Show More
khjang
USB EZ-PD™ Type-C
I am looking for CYPD3123 technical reference manual. In the process of analyzing the source code of CCG3,volatile uint32_t uvov_ctrl; /* 0x400a01c8 *... Show More
ScottL
USB EZ-PD™ Type-C
I am using the Infineon CY4535 EZ-PD evaluation kit to power a 5V, 3A device from a USB-C source. I find some portions of the documentation to be conf... Show More
bwhipple
USB EZ-PD™ Type-C
I seem to be unable to read or upgrade firmware using the EZ-PD Configuration utility. I'm following the "EZ-PD CCG3PA Evaluation Kit Guide" as well a... Show More
beewoo
USB EZ-PD™ Type-C
I am designing a board with that leverages DisplayPort over USB-C and hope to use the CYPD3120 part. The connectivity is - PC (DP source) -> DP to USB... Show More