USB EZ-PD™ Type-C Forum Discussions
text.format{('custom.tabs.no.results')}
I got CCG2 passive cable fw that contains two FW caycad.
one is main.cyacd, another is Failsafe.cyacd.
May i know what different between both of FWs?
if fw running in failsafe mode, are there any functional limitations?
Show LessHi Sirs,
Why HPI do not have example code could be shared?
If there are sample code , the development time can be shortened.
Will there be a chance to be open?
Thank you.
Show Less
Hi!
We are looking at a customer case where power supply for a USB-C PD 5A charger is 48VDC. Since it is hard (impossible) to find DC/DC-controllers optimized for USB-C with 48VDC we considered using a flyback solution instead.
Is it possible to use PAG1-solution with 48VDC input? We would of course not need the rectifier, but more or less keep the rest. Any other main things to consider if we were to base it on the 65W CoolGaN ref design?
/Olof
Show LessI am using EZ-PD Analyzer Utility Version 1.0.0.084 and although Windows recognizes the Cy4500 device, the application does not. This devices was working previously but stopped working recently. I have other CY4500 devices that have done the same. LED1 on the device flashes white when plugged in. I am unable to try reflashing the device because it is not recognized by the application. Is there another way to reprogram the device? Device sticker says 121-60321-01 Rev 09 2021CN00074. Thanks.
Show Less
My company is designing our own version of the CY4531 EVK. We will use the same CY7C65215 chip as the USB-to-I2C bridge to program the CCG3 chip. I assume the CY7C65215 needs a particular firmware loaded to support the CCG3, but I can't find any information about that the in EVK design documents. I also can't find any information on how to load the CY7C65215 with firmware. I don't have much experience with Cypress micros, so any information would be helpful.
Show LessTo whom it may concerned ,
a CCG2 is emplyed on our USB4 Gen3 cable product which undergoes the compliance test w/ 3 items failed —
1)Ra is out of 800 Ohm ~ 1.2K Ohm ( 3 pcs tested and 1/3 ok w/ Vconn @423 mV ,and 2 out of 3 NG w/ Vconn = 402 mV )
2) PD3 modes - checking SVIDs ( The UUT shall return a number of SVIDs in between 1 and 1, actual 2 (TEST.PD.VDM.CBL.1#3)
3)Checking Headers (Message ID 0): Manufacturer String shall be null terminated (COMMON.CHECK.PD.10#1 x 1)
Kindly advise the countermeasure of the above 3 issues.
f.y.i. 1)NG test report 2)SVID on VIF 3)SVIDs setting on CCG2 are on the attached photos。
Thank you and best Regards,
Alan Huang
Show Less
Base on KBA231336 https://community.infineon.com/t5/Knowledge-Base-Articles/EZ-PD-Barrel-connector-replacement-BCR-FAQs-KBA231336/ta-p/289954
But we can not find any information about CYPD3176 & CYPD3178 on web.
Please kindly share datasheet, HPI Spec. , UFP SDK etc.
Current we want use CYPD3176 to support PPS sink application.
Show LessHi Cypress,
I now use CYPD4226 & CYPD4236.
In some situations, I want to turn the device into an only USB device without PD.
Can I use API or HPI to close PD communication, but Rd is still Pull Down?
Thanks!
Show Less