USB EZ-PD™ Type-C Forum Discussions
Hi This is the model info I am using: CYPD5225-96BZXI (CCG5)
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/PSoC-5-3-1/%E5%A6%82%E4%BD%95%E8%A7%A6%E5%8F%91%E5%8D%8F%E8%AE%AE%E5%8F%8C%E6%96%B9%E9%87%8D%E6%96%B0%E5%8D%8F%E5%95%86pdo/m-p/697947
Show LessHello Support,
Thank you for your ususal support.
I have a question of CCG3.
Does the CCG3 support Embedded Display Port on AlteranteMode??
Best reagrds,
Koki
Show Less
Can IEC 62368-1 and UL certificates for CCG6SF / CCG6DF be provided?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/USB-EZ-PD-Type-C/CCG6-IEC-62368-1-%E5%92%8CUL/td-p/694523
Show LessI am designing the 65W usb c type charger using CYPAS111A1 PAG1S . I want to cut off the usb output via a controller. does holding the ic to reset via XRES pin power down the ic's final output? kindly support with this.
Show Less
In a previous ticket, we resolved the issue with the general USB 2.0 connection after a cold start. The solution was an FW update to version CYUSB4347-BZXC_FW_2_0_0.bin
The update solved the general problem but created a new one...
Since the update, PORT1 on CYUSB4347-BZXC always connects only with USB2.0 slow speed. I tried to compare the configuration file between PORT0 and PORT1 but I didn't find any significant differences. The other ports always work correctly.
Is it a known bug? Can you please check what can be the reason for this behavior or recommend some settings I can check in the configuration file?
Please find the log file in attachments. (The line "Finished FW update process with status COMPLETED PARTIALLY (0x4)" is a new thing, I am unsure of its significance, but the hub is functioning properly.)
If you need any more information, I would be more than happy to provide it for you!
Thank You!
Kristian
Show Less
Is there a way to read out all power profiles of a PD source with the CY7110 EZ-PD PMG1?
It would be great, if there is a way to connect a USB supply (PD) to the kit and the kit returns all possible profiles, which the supply provides...
Show Less
Because customer has some special requirement, so the PD FW has to implement some customized functions.
so we would like to use CCG6 - CYPD6127 for this Meteor Lake, it flash size is big than CYPD6227
Becuase The latest version of Host SDK is ver 3.6 that doesn't support this CYPD6127 part.
so can i use SDK 3.5 for Meteor Lake platform ??
SDK 3.5 - platform selection has "MTL" key word :
Show Less
Hello
We're encountering an issue when attempting to charge a Samsung S8 tablet via a USB Hub plugged into a Type-C port while the tablet's battery is dead. We have raised a ticket for a similar issue, which can be found at the link below
S8 Charging issue when connected to the USB Hub via a Type-C port.
This solution allows us to charge tablets, however we are not able to charge tablets if their batteries are dead (below 0% ).
Please help me in this situation
Show Less