Announcements

Live Webinar: USB-C adoption. Simple & Cost-efficient solutions | April 18th @9am or 5pm CEST. Register now !

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB EZ-PD™ Type-C Forum Discussions

NirAlon
USB EZ-PD™ Type-C
Hello, I am interesting in evaluating the CYPD3120 in a DisplayPort application.I've noticed there is a reference design called "EZ-PD™ CCG3 USB-C to ... Show More
PrRe_3492461
USB EZ-PD™ Type-C
Hello community, I'm using CCG3PA for my product development.It can act as only PD/QC Sink. So to verify Qc 2.0 Sink Functionality I'm using miniprog ... Show More
role_1685151
USB EZ-PD™ Type-C
Hello. IFX. I can see that Auto CCG7D supports PD3.0 in datasheet. Customer asked whether Auto CCG7D supports PD3.1 specification. Please check it? Re... Show More
Rach_Ni
USB EZ-PD™ Type-C
Dears Please help to recommend a PD protocol chip with high cost performance, which is used in charger application scenarios, only for the source side... Show More
JPS
USB EZ-PD™ Type-C
Discussion started in case 0668800.  We unsuccessfully try to modify a board CY7111 to run it as a USB PD Source (i.e.: charging a phone). The PMG1-S1... Show More
td83
USB EZ-PD™ Type-C
Hi, When using the firmware/binary file provided by Cypress CYPD5225-96BZXI_notebook_3_4_0_2559_0_0_0_nb.hex the device CYPD5225 fails to decode an I2... Show More
td83
USB EZ-PD™ Type-C
Hi, With PSoc creator, i am using the Cypress code example "CYPD5225-96BZXI_notebook_tbt".In the "pins tab" some pins of the device CYDP5225 have no c... Show More
td83
USB EZ-PD™ Type-C
Hi, I am using the .HEX file found in the directory <<Install directory>>\Cypress\EZ-PD CCGx Host SDK\CCGx\Firmware\binaries\CYPD5225-96BZXI_notebook_... Show More
DaEr_349131
USB EZ-PD™ Type-C
Was planning to let the CCG5/6 do some additional "SMC" type monitoring in a system,  i.e. hook up some high-side precision sensing + ADC's (I2C + SPI... Show More
CYW20719
USB EZ-PD™ Type-C
您好:我这边有个客户想实现UFP+SOURCE的应用,不知道这个原理图上有没有什么问题,P2.2需要在协商时给出一个低电平,复位hub。客户想要使用SWD,SCLK做下载口,在这种情况下如何通过configuration utility配置UFP. Show More
Forum Information

USB EZ-PD™ Type-C

Discussion forum regarding USB EZ-PD™ Type-C topics.