USB EZ-PD™ Type-C Forum Discussions
text.format{('custom.tabs.no.results')}
Hi,
Good day.
May i know where is able to download the programming guide of CCG8D/S?
Could you help to provide the programming guide for CCG8D/S series to us?
Thank you.
Jack Hsu
Show LessAs we known, we can program firmware with Miniprog,
I just want to know CCG5 CYPD5225 if can use Segger or ST Link to program hex file?
I tried Segger and STLink to programm CYPD5225 but failed.
Show LessIs it possible to log Voltage and Current values from CY4500 EZ-PD Protocol Analyzer to an excel?
Hi All,
We are developing a custom USB-PD solution using CYPD3175 & ACT4751. But we are not getting a USB to connect/disconnect events or make a call to psource_set_voltage. Thus VBUS is charged at default 5V.
We are not using VCONN, and CC/D+/D- lines are connected to CYPD3175, Attached are config files.
We would also like to know
1. How to generate a PDO table when we used the EZPD Config utility saving results in a format error.
2. How to read external ADC PIN e.g. P2.1. (there is no ADC block in components)
If required, we can share our schematic and source code through the mail
The CCG7D contains Buck-Boost Controller function.
and it can be configaured by ez-pd configuration utility.
Can you please provide parameters tuning guide and doucment to exaplain those parameters in detail?
Show Less
CY7113 키트를 사용하는데 PMG1-S3에서 140W(28V5A)를 적용할 수 있는 방법이 궁금합니다.
Using CCG5 as the sink end, The Apple 20W or other 65W PA charge for ccg5, a hard reset occurs when PA plugin, PD LOG has been posted.
Please help to analyze the reason.
Show Less
Hi,
In my design Iam using CYPD4126-40LQXIT IC. As per my application requirement, IC power role will be Provider so I have to VBUS_P_CTRL_P0/P1.6 this signal to enable VBUS provider path, as Iam not using Consumer role, DoI need to use VBUS_C_CTRL_P0 this signal, can I left open?
Show LessHi community,
I am using CCG3PA it works as PD 3.0 source, Can I be able make it work as PD 2.0 source ,can i reduce the USB-PD spec revision to 2.0.
Can you give me an insight on function responsible for making CCG3PA function as PD 2.0 source?
Show Less