USB EZ-PD™ Type-C Forum Discussions
Base on datasheet https://www.cypress.com/file/500276/download
You have show CCG6SF 96-BGA footpront.
But ordering information no CCG6SF BGA package part number.
If CCG6SF have 96-BGA parts, it will helpful for co-design one port & two port with same PCB layout.
Please kindly to have comment & suggestion for this concern.
Thanks,
Mitchell
Show Less
Hi Everyone,
I would like to ask , is source code of CY6611 EZ-USB HX3PD EVK available?
Is it possible to program CY6611 EZ-USB HX3PD EVK through source code?
Thanks,
Liwan
Show LessLinux analyzer utility shows empty data(screenshot attached), while the Windows version works fine on same analyzer HW.
Linux version:
Linux XXXX #60~20.04.1-Ubuntu SMP Thu May 6 09:52:46 UTC 2021 x86_64 x86_64 x86_64 GNU/Linux
java version "1.8.0_291"
Java(TM) SE Runtime Environment (build 1.8.0_291-b10)
Java HotSpot(TM) 64-Bit Server VM (build 25.291-b10, mixed mode)
EZ version:Cypress Semiconductor Corporation
CY4500 EZ-PD™ Protocol Analyzer Utility
Version : 3.1.0
Build : 31
Copyright © Cypress Semiconductor 2020
Thank you very much.
Show LessWe have a lot of PCBA board failures.
After FA analysis, the FA report result always is EOS in CCG4 Vddd / Vddio pins.
Do you have any suggestions to protection it ??
Show LessHi Team Cypress/Infineon,
Any chances we could see the CCG series go open source anytime soon?
Curious to understand the reasoning behind why all these parts are closed source / hex releases only
I mean, very little risk of taking anything to another platform as the "psoc" running it is fairly unique in it's peripheral-set.
Also, many other PD PHY vendors have full open-source PD stacks including the TCPC abstractions layers.
Hi!
We are deploying adapters based on CYPD3123 and we use USB bootloader for firmware updates. Now we would like to add support for encryption of these firmware images so not anyone can update them in the field.
Is there a guide on how to set this up?
Cheers
Olof
Show LessIf the CCG3120 is unpowered from either VSYS or VBUS and HPD is high, is there any concern or risk of damaging the device?
Based on our measurements I think in this state VDDIO will be back powered through internal body diodes. Is this a safe condition to be in?
This is an easy condition to enter if the ccg3 is unplugged from the host, but still attached to a monitor.
Since we were externally powering VDDIO - we noticed that this would cause the CCG3120 to get in a bad state.
Show LessHi!
We use the CCG4 in our dock design, but need to add a billboard controller as well. We are using the EC/HPI I2C interface to communicate to our central MCU and we don't need the full DMC functionality so we don't want to use the design used in the CCG4 dock ref design. Is there a guide on how to integrate e.g. CY7C65210 with CCG4 in a way that it does not conflict with the EC/HPI interface?
Cheers
Show Less