Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB EZ-PD™ Type-C Forum Discussions

USB EZ-PD™ Type-C Forum Discussions

Sort by:
sh
USB EZ-PD™ Type-C

CY7113 키트를 사용하는데 PMG1-S3에서 140W(28V5A)를 적용할 수 있는 방법이 궁금합니다.

GrCa_1363456
USB EZ-PD™ Type-C
What is the process to revert a CY4500 USB-C Analyzer back to its original firmware, 1.0 that supports USB-C PD 2.0? Only the original firmware, versi... Show More
profhell
USB EZ-PD™ Type-C
Dear all, First of, apologies if I've missed this as a FAQ, but haven't been able to find a similar query. I'm looking into designing a multi-port rea... Show More
dlachance
USB EZ-PD™ Type-C
Hello Infineon, Pin 24, VCCD which is the output of an internal 1.8V regulator for internal logic, comes up to about .9V and slowly drains down to 0. ... Show More
Mitchell_shen
USB EZ-PD™ Type-C
Base on application note mention "The dead battery Rd resistors are disabled by the application firmware once the device is powered up." But we want t... Show More
Davidg25
USB EZ-PD™ Type-C
I have found some stock in a CCG4 part but there are some extra characters at the end of the part number.  Does anybody know what these extra characte... Show More
joa_4818671
USB EZ-PD™ Type-C
Hi We are working on a device that needs the ability to charge connected devices and if a data connection is present (at UFP) act as a hub. (while cha... Show More
nyoung
USB EZ-PD™ Type-C
We are trying to get a design working with display port over USBC. We are using an adapter to attach the DP monitor and power our device. The firmware... Show More
JamesShih
USB EZ-PD™ Type-C
Hi, I'm working on a custom board which is based on H3XPC EVK and replace the NCP81239 (2PD) to NCP81231(1PD), in this design, PD port only has 1 and ... Show More
KiLe_4629881
USB EZ-PD™ Type-C
Hi Cypress,   We have a design that is using the CYPD5225 with TGL and a burnside bridge retimer on each port, however after the system exits S4/S5 af... Show More