USB EZ-PD™ Type-C Forum Discussions
Hi Infineon team:
I am designing a DRP application, which can be used as a power provider or a power consumer.
as shown below.
The requirement is to support PD3.1 and extended power range (EPR).
It can be seen from the official website that PMG1-S3 meets the requirements. But it is out of stock. Is this chip in commercial use?
Are there any other chips that can be used instead?
Apple's 140W charger uses CYPD3135, but the datasheets of CYPD3135 only support PD3.0. Is it a customized update? So we should not be able to use it?
Show Less
Hi,
I'm using CYPD3175 with MAX25430 in my design.
does any one used this combination before?
now i dont have any clue how to use CYPD3175 to communicate with MAX25430.
is there any example i can find? Thanks!
Show LessHi. Infineon
customer want to use CYPD5225-96BZXI 4* GPIOs to directly driver 4LED, the each LED maximum driving current is 5mA. the mode use open drain, drives high input(target:consider cost, without add other driver IC). in datasheet (page22)(Table 8. Absolute Maximum Ratings[8]), IGPIO_ABS(Maximum current per GPIO) max is 25mA.
my question: whether CCG5 's one GPIO can drive one LED?
thanks
flance fang
Show LessHi there,
In CCG7DC webpage has a reference "Test Report 65W CCG7D 2C Buck Solution Board with By Pass FCCM",
Is there schematic and Gerber file we can provide to use?
I know in document there are sch and gerber pics, but it's roughly and not much useful
Thanks
Show Less
我使用的是 CYPD4226 芯片,我在笔记本的例程中使用了 noboot 项目,最初使用 miniprog3 进行编程调试,但它不可用于现场升级。 我发现笔记本的项目也有 i2c 引导项目,我已经阅读了有关引导加载程序和可引导加载的文档。 现在我想使用不同的MCU并通过I2C接口进行现场升级。
我有以下问题:
1. 该芯片可以与其他MCU通信并现场升级吗?
2. 如果是,你能指导我怎么做吗?
Show LessHi there
請問CCG3PA是不是不能用miniprog4在IDE裡使用online debug?
在community裡很多討論IDE debug的問題,答案卻都不一樣
謝謝
Hi,
I have the CCG3PA EVK (CY4532). By default, it is configured as source. In EZ-PD Configuration Utility, I see the "Port Role" set as "Source". I am trying to set the EVK to a sink-only configuration to prototype my application. However, the drop-down menu is greyed out so it won't let me change the option away from "Source".
1. How do I get EZ-PD Configuration Utility to provide the "Sink" option since it is greyed out by default?
2. My sink configuration will request only 1 sink profile when connected to a multiple source PDO device. Will adding a specific "Sink PDO" in EZ-PD Configuration Utility be the solution? Right now, there are no Sink PDO options displayed, but I am assuming it is because the "Port Role" is set to "Source".
Thanks,
Jonathan
Hi,
Gatkex Creek's FW update tool for Mac was working over libusb, when customer would like to install it by manual that which version of libusb is required?
Is it possible of IFX to repackage FW update tool with libusb of of static-library? If it is possible, end customer will not need to install it by manual when customer's MacOS no libusb.
BR
Eason
Show Less当我使用外部MCU进行引导加载程序时,我需要发送的文件数据是来自.hex文件还是a.cyacd文件?