USB EZ-PD™ Type-C

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
PaRi_1293246
USB EZ-PD™ Type-C
Hello, We have implemented a DRP with the controller CYPD3125 and the Mux PS8743B because the Mux PS8740B is not recommended for new design.  The CYPD... Show More
sims
USB EZ-PD™ Type-C
Hi there, Could you provide ez pd protocol analyzer utility build with openJDK ? Cause oracle jdk policy is restricted to commercial use. My company I... Show More
etye_3732486
USB EZ-PD™ Type-C

Hi,

Could you please tell me the TID of CYPD3174-24LQXQ  ?

Best Regards,

Alex

 

PhienNguyen
USB EZ-PD™ Type-C
Hi, I have a project as below: - CYPD3174 work in no feeback mode. - MCU read PD contract negotiation from CYPD3174 and set voltage to ACT4751. 1. To... Show More
BHeumueller
USB EZ-PD™ Type-C
Hellowe are currently working on a design using Thunderbolt with a CCG5 USB-C Power Delivery controller. Our reference design is Tapex Creek. On your ... Show More
kirankalsani
USB EZ-PD™ Type-C
Hi, I would like to confirm if every cypress PD Device CYPD6227-96BZXI programmed with basic firmware when the part is shipped out from cypress factor... Show More
NoAr_1540581
USB EZ-PD™ Type-C
Hello   The CC pin and VBUS are exposed when viewed from the outside, such as when Type-C is inserted and removed continuously, and when the connector... Show More
pleasework
USB EZ-PD™ Type-C
Hi, I am trying to use the CYPD3177 over I2C to control a USB-PD SRC. After connecting a USB-PD 100W supply: - FLIP signal rises from 0 to 3v3 - USBPD... Show More
td83
USB EZ-PD™ Type-C
Hi, We are using a Tigerlake SOC with a CYPD5225 power delivery. I have checked the I2C bus between the Tigerlake and the CYPD5225, there is I2C acces... Show More
Ping
USB EZ-PD™ Type-C
Dear Sir/Madam, Please help to check the CYUSB4347 USB3.1 Gen2 (10Gbps) Hub is there suitable for the below application. CYUSB4347's UpStream port att... Show More
Board Information

USB EZ-PD™ Type-C

Discussion forum regarding USB EZ-PD™ Type-C topics.
Top liked authors