Announcements

Live Webinar: USB-C adoption. Simple & Cost-efficient solutions | April 18th @9am or 5pm CEST. Register now !

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB EZ-PD™ Type-C Forum Discussions

Jiong
USB EZ-PD™ Type-C
Hi,   请问下我在使用PSoC Creator4.4打开电脑文件路径“C:\Program Files (x86)\Cypress\EZ-PD CCGx Host SDK\CCGx\Firmware\projects\CYPD4226-40LQXI_notebook\CYPD4226-40LQX... Show More
Ivan_Lee
USB EZ-PD™ Type-C
  Customer would like to develop a C to DP / DP to C "bidirectional" dongle using CYPD3120  Can you please provide us the reference firmware and hardw... Show More
PrRe_3492461
USB EZ-PD™ Type-C
Hello Community, I'm able to configure 5A in SrcCaps only for Fixed Supply type PDOs, If I want to configure 5A for APDO supplytype, I'm unable to con... Show More
Jiong
USB EZ-PD™ Type-C
Hi,   我在使用 1.3.7版本的EZ-PD configuration utility 的时候,生成的文件有三个,一个是.c后缀,一个是.cyacd后缀, 一个是.xml后缀的文件,然后我在看这个文档的时候“EZ-PD Configuration Utility User Manual.pdf... Show More
txcao
USB EZ-PD™ Type-C
Hello, There are examples for each IC on CCGx SDK 3.0.2 I would like to ask if there is any guide or examples to use CYPD3120 in the upstream mode an... Show More
64bittz
USB EZ-PD™ Type-C
Hi, in my application I need roughly constant power, about 8W. This means that the current changes significantly from 5v to 20v, at which the circuit ... Show More
SoU_4942226
USB EZ-PD™ Type-C
Since I am considering the Artwork design of PMG1-S3 (CYPM1311), Please tell me the maximum allowable current value of 31pin VBUS-C of CYPM311. Show More
txcao
USB EZ-PD™ Type-C
- Example code: Any example code for CYPD3120 or CYPD3123 - PSoC version: 4.4 or 4.5 - PSoC IDE setting: + If using default ARM toolchain: ARM GCC 5.4... Show More
JoLu_3455101
USB EZ-PD™ Type-C
Hi, I have a CYPD3171 Sink-only application modeled after the Power Bank example, but without internal battery. So this is a sink-only application. Th... Show More
Forum Information

USB EZ-PD™ Type-C

Discussion forum regarding USB EZ-PD™ Type-C topics.