Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB EZ-PD™ Type-C Forum Discussions

USB EZ-PD™ Type-C Forum Discussions

Sort by:
Xuesong
USB EZ-PD™ Type-C
hi 我需要修改CYPD5225-96BZXI_notebook_tbt案例工程来 配合Goshen Ridge IC,由于我们的hardware设计不同 ,需要把案例中的RTM I2C和 RETIMER_PWR_EN_P1、RETIMER_FORCE_PWR_EN.......等如图中的去掉,去掉... Show More
Ivan_Lee
USB EZ-PD™ Type-C
We use CYPD6227  (CCG6DF) two port PD controller ( Port 0 and Port 1 )  to implement alder lake platform. but actually our project is single type-c po... Show More
BSlava
USB EZ-PD™ Type-C
Hello, I have multiple DMC chips in my system with the same VID/PID connected to the same computer, each with its own unique serial number. Unfortunat... Show More
Ivan_Lee
USB EZ-PD™ Type-C

 

Could you please provide us the CCG8 datasheet?

 

Ivan_Lee
USB EZ-PD™ Type-C
  1. Does Host SDK support Intel Maple Ridge platform?    if supported, which SDK's project is used for Maple ridge ? 3. another question , what diffe... Show More
liam
USB EZ-PD™ Type-C
CY4500 Driver
Solved
Dear all,   Can you send me the driver of CY4500, to Liam.liu@corp.ovt.com I also cannot found the driver folder after installed the EZ-PD Protocol an... Show More
User22355
USB EZ-PD™ Type-C
Hi all, I am using the CYPD3177 in a custom design. When the plug is connected, I receive the Vcc (1.8V) supply but not the VDD (3.3V) supply. The Vbu... Show More
NoAr_1540581
USB EZ-PD™ Type-C

Hello

Could you please tell me the Silicon ID of CYPD6128-48LQXI?

 

Best Regards

Arai

cshin
USB EZ-PD™ Type-C
Hello, Can I use two I2C buses simultaneously in a CCG3PA device? One is for host communication and the other is for an external DAC access. The CCG3P... Show More
NoAr_1540581
USB EZ-PD™ Type-C
Hello I would like to detect the connection/disconnection status with the HOST device and output a (GPIO) signal to the external EC. In details, Speci... Show More