Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB EZ-PD™ Type-C Forum Discussions

USB EZ-PD™ Type-C Forum Discussions

Sort by:
cshin
USB EZ-PD™ Type-C
Hello, Can I use two I2C buses simultaneously in a CCG3PA device? One is for host communication and the other is for an external DAC access. The CCG3P... Show More
Yee6
USB EZ-PD™ Type-C

Could you share me a link that is project FW based on CCG4?

julius_yang
USB EZ-PD™ Type-C
please help check the follow problems: 1、When we test 5V/3A, 9V/2A,the OCP trigger is below: a、Expect test results: 5V/3A: 3A * (1 +10%) = 3.3 A  ,   ... Show More
Ivan_Lee
USB EZ-PD™ Type-C
  1. Does "VBAT to GND protection" and "VBUS OCP" use the same - resistor current sensor to detect  current ? ( pin#18 and pin#19) 2.  Application not... Show More
leosun
USB EZ-PD™ Type-C
  SDK version: ezpdhostsdk_3.4.0_Windows_x86-x64.exe .... .\CortexM0\ARM_GCC_541\Debug\hal_ccgx.o .\CortexM0\ARM_GCC_541\Debug\pdss_mx_hal.o .\CortexM... Show More
HuHong
USB EZ-PD™ Type-C
Hi ,   I have a question about CCG5 source Vbus OCP。When ocp_cur is 3A,only 3.8A  above can trigger OCP .   Normally,3.3A can trigger ,but not functio... Show More
NoAr_1540581
USB EZ-PD™ Type-C
Hello https://community.infineon.com/t5/USB-EZ-PD-Type-C/about-the-PMG1-S3-power-supply-for-Vsys-Vbus-c-p0-Vbus-c-p1/ m-p/367578#M7177 Regarding the a... Show More
HuHong
USB EZ-PD™ Type-C
We implement PPS sink on CCG5,follow by Solved: PPS Request for specific Voltage - Infineon Developer Community 1.The function hpi_set_userdef_write_h... Show More
Moon_shi
USB EZ-PD™ Type-C

针对TYPE-C PD 3.1 的UFP,BCR我们有方案可以支持吗?BCR 支持PD3.1的产品有更新计划吗?

Thanks & Best Regards,

Moon

liam
USB EZ-PD™ Type-C
CY4500 EZ-PD
Solved

JAVA is required during the software installation of CY4500 EZ-PD protocol analyzer. Is this JAVA charged for commercial use?