Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB EZ-PD™ Type-C

Recent discussions

Sort by:
MaKe_4459911
USB EZ-PD™ Type-C
To confirm that the bootloader is running, I'm toggling 2 GPIO pins to indicate that I've entered main() in the bootloader.  If I build the bootloader... Show More
BhargavGolla
USB EZ-PD™ Type-C
Hi, I am using CCG3PA board in my device to work  as PD source and QC source. It was working as PD source fine but it is not working as QC source when... Show More
Chenjun
USB EZ-PD™ Type-C
我使用型号是:CYUSB3013,现在通过GPIO53~56作为串口,使用官方的例程,不能输出信息。官方工程连接:https://www.cypress.com/documentation/application-notes/an75779-how-implement-image-sensor-interface-using-ez-usb-fx3-usb Show More
Harry
USB EZ-PD™ Type-C
I'm working on the firmware of CYPD5235-96BZXI.I hope I can change PDO settings butthe "EZ-PD configuration utility" doesn'tseems support my chip.Then... Show More
Ivan_Lee
USB EZ-PD™ Type-C
  Customer use CCG7D and IPZ40N04S5L-4R8 to design Rear-Seat Charger. now they have two questions about temperature, because currently the MOS Surface... Show More
role_1685151
USB EZ-PD™ Type-C
Hello. I wonder if it's possible to use CCG4 device for CTD application. Infineon's CTD design recommended to use CCG3 + CCG2. but CCG4 have 2 PD cont... Show More
PaRi_1293246
USB EZ-PD™ Type-C
Hello, I have installed PSoC Creator 4.5 and ARM Keil MDK v5.37. When I compile the project CYPD3125-40LQXI_notebook, that is the project for the CCG3... Show More
Ivan_Lee
USB EZ-PD™ Type-C
Hi, Sir,   I have a intel Alder-Lake platform project, and customer is design schematic using CCG5C.   Dose Host SDK - CYPD5126-40LQXI_notebook_tbt pr... Show More
hoperobin
USB EZ-PD™ Type-C
Hello, I am working on a design that is using CYPD6125-40LQXIT in a consumer device for 20V at 5A. The schematic as it is now is connecting Vbus on th... Show More
PaRi_1293246
USB EZ-PD™ Type-C
Hello, We have implemented a CYPD3125 on our latest ultrasound scanner.  We use the firmware of the evaluation kit with some modifications to the conf... Show More