Announcements

Live Webinar: USB-C adoption. Simple & Cost-efficient solutions | April 18th @9am or 5pm CEST. Register now !

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB EZ-PD™ Type-C Forum Discussions

MaGa_3860551
USB EZ-PD™ Type-C
Hello,We are using the CCG3 CYPD3125-40LQXIT with a custom notebook firmware based on the notebook example of the SDK 3.2.1, and we're having some str... Show More
MiMu_4671456
USB EZ-PD™ Type-C
We want to provide power using USB-PD to a device with custom (waterproof and durable) connectors.Ideally we also want to transmit data and/or video, ... Show More
JiLu_4664471
USB EZ-PD™ Type-C
The VBUS_in_discharge pin has 30V rating, but the bus voltage is 21V maximum.Is there a specific reason to have such a high voltage rating on this pin... Show More
AnGa_4482271
USB EZ-PD™ Type-C
Hello,There's this function in power_bank.c, in the CYPD3171_pb example code:static uint16_t pb_get_battery_voltage(void){    /* Measure voltage on VB... Show More
BiBr_4663101
USB EZ-PD™ Type-C
I've read in other discussions that a bypass capacitor should be placed across the Rsense resistor to reduce noise. Is a 100nf 50V MLCC cap good to us... Show More
GrCa_1363456
USB EZ-PD™ Type-C
Where are the PSoC Creator Project Files for the various CCGx parts?I'd like to make minor modifications to the Bootloaders on a CCGx part. I understa... Show More
PrRe_3492461
USB EZ-PD™ Type-C
Hello All / RajathB_01​I'm using CCG3PA DVK kit.I want to configure ccg3pa's Snk capabilities in Runtime.I know how to configure using configuration u... Show More
JaPh_4533531
USB EZ-PD™ Type-C
Hi,I'm using a CYPD3177 and I'd like to be able to communicate with it over an I2C bus. The device datasheet doesn't have any information about regist... Show More
GrCa_1363456
USB EZ-PD™ Type-C
Regarding KBA219845 @ https://community.cypress.com/docs/DOC-13701I tried to work through KBA219845 and ran into questions with step 5.Step 5 appears ... Show More
NoAr_1540581
USB EZ-PD™ Type-C
HelloAfter confirming the VCONN request, in case of 3A or more, VCONN needs 1W capacity to supply power to e-Maker.Q1) When connecting a cable with eM... Show More
Forum Information

USB EZ-PD™ Type-C

Discussion forum regarding USB EZ-PD™ Type-C topics.