Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB EZ-PD™ Type-C Forum Discussions

Recent discussions

Sort by:
KyleWK
USB EZ-PD™ Type-C

What is TID of CYPD4236-40LQXIT?

Please provide it.

Regards, Kyle

chch_3621411
USB EZ-PD™ Type-C
Hello world, so i have a project of 2 port USB-C powerbank,  each port as it own CYPD3171-24LQXQ they work independly but i want to connect them using... Show More
jast_4281081
USB EZ-PD™ Type-C
My goal is to create a very low-cost converter that charges a USB Type C device from an existing 20V DC supply. My converter will have 20V input and U... Show More
HaG_2273236
USB EZ-PD™ Type-C
Hello Members,We are using CCG3PA in consumer mode only. Need information on below pins 1. VBUS_C_MON_DISCHARGE   --> This pin used to Monitor VBUS Vo... Show More
jachc_1409281
USB EZ-PD™ Type-C
CYPD3171-24LQXQ本体丝印说明第一行和第二行是型号,但第二行一横后面没有数字,现我手上样品为第一行为CYPD,第二行为3171-2,有些样品第二行为3171-C。请问横杠后面的表示什么?能否提供芯片丝印说明? Show More
SaBh_294166
USB EZ-PD™ Type-C
Hi. We will be using a CCG3PA in our design. Also wanting to have the ability to program a fresh PCBA over SWD either at the factory or when out in th... Show More
kehsc_348861
USB EZ-PD™ Type-C
Hi, I have a question about market format of CYPD5225-96BZXIT.I cannot find market format of CYPD5225-96BZXIT on CYPRESS GENERAL MARKING FORMAT_APRIL ... Show More
NiMc_4245981
USB EZ-PD™ Type-C
I'm trying to decide if I can update our CCG3 device through the exposed Type-C port.  Will external hardware be required, or can I connect directly t... Show More
pavec_4247266
USB EZ-PD™ Type-C
hello i have this whole question:i downloaded the power bank reference design PB-811 and i removed the USB-A i have kept the micro usb for charging an... Show More
xizh_4275346
USB EZ-PD™ Type-C
Display cannot work when using our USB3.1 TypeC active cable to connect display and NB which uses CYPD4255-96BZXI as USB interface IC.  It seems that ... Show More
Forum Information

USB EZ-PD™ Type-C

Discussion forum regarding USB EZ-PD™ Type-C topics.