USB EZ-PD™ Type-C Forum Discussions
About CYPD2122-24LQXI Plating Ball
Originally, there are 2 kind of plating ball?
NiPdAu
PureSn
Was this from the beginning?
Or is PCN on the way?
No such PCN could be identified.
Show LessQ: where i could find address of each part in FLASH Memory
Q : when i load hex file i update only fw application or also configuration table area ?
Show LessIn example power adapted direct or class projects when enable above macro.the build failed
Hi,
When I used mini B cable to connect PC and CY4531 CCG3 Evaluation board,at the same time, I powered on CY4531, Device Manage of PC can detect device,displaying "USB-serial adapter1" and "USB-serial(dual channal) vender MFG". But on the EZ-PD Configuration Utility, it can not find the HID/USB-serial Bridge devices and displayed "
0 HID devices found
0 USB-Serial Bridge devices found
No HID/USB-Serial Bridge devices found
Device Discovery failed"
So any ideas? And must I use miniprog3 to debug program?
If I use miniprog3, can the EZ-PD Configuration Utility detect device?
Thanks.
Show LessHi there,
I have something a little strange happening when I attempt to read/write a new configuration to the CYPD3120. It only occurs when using the bootloader to read the configuration on the currently active firmware. It also has a similar problem when trying to use the bootloader to update both firmwares at the same time.
In short, it looks like the CYPD3120 enters the bootloader with no trouble.
The Message window reads:
Starting CCG configuration read over HID interface.
Jump to Boot command successful.
It will then wait there for around 30 seconds before giving me a failure messagebox "Configuration read failed".
The Message window at this point shows:
Error: Failed to find handle to HID Device
Error: Failed to read CCGx configuration.
Error: DLL call returned error while reading the configuration
However, if after the Jump to Boot command successful message I power cycle the CYPD3120, it reads out the configuration with no problems.
Reading the configuration of the firmware that is not currently active has no problems at all.
Anyone know why this might be or how to fix it?
Show LessHi,
When I used mini B cable to connect PC and CY4531 CCG3 Evaluation board,at the same time, I powered on CY4531, Device Manage of PC can detect device,displaying "USB-serial adapter1" and "USB-serial(dual channal) vender MFG". But on the EZ-PD Configuration Utility, it can not find the HID/USB-serial Bridge devices and displayed "
0 HID devices found
0 USB-Serial Bridge devices found
No HID/USB-Serial Bridge devices found
Device Discovery failed"
So any ideas? And must I use miniprog3 to debug program?
Thanks.
Show Lesscy4532 bootable project usage sprintf function cause error build
include <stdio.h>
sprintf(debug_buff,"%2x",dpm_voltage); in main file
error build image
Show Lessprogramming CYACD file from from example SDK CCG3PA Car Charger (CLA) with EZ-PD™ Configuration Utility broken PD contract and failed read configuration device CYPD3175 and failed update FW
Q: does any update need in FW sdk in order EZ-PD™ Configuration Utility read device ?
only when programming device witrh CYPD3171-24LQXQ_cla_3_4_0_2274_0_0_0_pa.hex with SWD interface only then it is possible to read configuration device
Show Less