Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB EZ-PD™ Type-C Forum Discussions

Sort by:
MuIc_4620061
USB EZ-PD™ Type-C
Hi,USB-PD Thema. What is responsible for generating different voltages at VBUS? Is it not the CCGX chip, right? If a UFP needs 20V and negotiates with... Show More
TeMa_2997106
USB EZ-PD™ Type-C
当該デバイスはBC1.2のCDPをサポートしていますでしょうか。D+/D-端子はシステムでも使用したいため、CDPモードにしたいのですが、明確にサポートと謳われているのはCCG5/5Cのみのようで、こちらをチョイスすべきなのか否かの判断をしたいです。 Show More
ArPa_4534921
USB EZ-PD™ Type-C
Hello, Is there an SDK for CY4500 EZPD but for the MicroB port? We would like to develop our own application for packet capture instead of EZ PD captu... Show More
JaVu_4007791
USB EZ-PD™ Type-C
Hi,In continuation to my previous thread "Unable to charge a dead battery tablet"How can i force charge a device (say with 5V 1Amp) by CCG3 PD and not... Show More
NoAr_1540581
USB EZ-PD™ Type-C
HelloQ1) CMG1 has a built-in 40-byte storage area for configuration. Ibut s this flash?Q2) Also, it is considered that the memory area other than the ... Show More
brzh_4088906
USB EZ-PD™ Type-C
I want to update firmware for Cypd3125 throng I2C, I don't know how to do ? Anybody can help me?block: PC ->  Cypress 65215 -->CYPD3125 Show More
SaBh_294166
USB EZ-PD™ Type-C
Hello. Happy New Year to all.Is the CMG1 component TID certified? PD3.0 compliant? Stable without any erratas? In production?Our company is interested... Show More
RaRo_1233086
USB EZ-PD™ Type-C
We are in need of a simple single voltage PPS request for CYPD3171 SDK 3.3 , our customer has an 11V requirement on his device and the power adapter t... Show More
MaLi_3529141
USB EZ-PD™ Type-C
Dear,I made a dock and used the CYPD4236-40LQXI_dock sample code.Connect to a host, CC can't communicate, fail rate is about 60%.But on other hosts, n... Show More
NaWo_4517846
USB EZ-PD™ Type-C
We're working on a small project in which we'd like to implement a UFP into our power system and was hoping to get some guidance before heading too fa... Show More
Forum Information

USB EZ-PD™ Type-C

Discussion forum regarding USB EZ-PD™ Type-C topics.