USB EZ-PD™ Type-C

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
pleasework
USB EZ-PD™ Type-C
Hi, I am trying to use the CYPD3177 over I2C to control a USB-PD SRC. After connecting a USB-PD 100W supply: - FLIP signal rises from 0 to 3v3 - USBPD... Show More
td83
USB EZ-PD™ Type-C
Hi, We are using a Tigerlake SOC with a CYPD5225 power delivery. I have checked the I2C bus between the Tigerlake and the CYPD5225, there is I2C acces... Show More
Ping
USB EZ-PD™ Type-C
Dear Sir/Madam, Please help to check the CYUSB4347 USB3.1 Gen2 (10Gbps) Hub is there suitable for the below application. CYUSB4347's UpStream port att... Show More
NoAr_1540581
USB EZ-PD™ Type-C
Hello   The CC pin and VBUS are exposed when viewed from the outside, such as when Type-C is inserted and removed continuously, and when the connector... Show More
Eric_K
USB EZ-PD™ Type-C
Is there a 3D model of the PCBs contained in the CY4531 EZ-PD CCG3 Evaluation Kit?  I would like to have a .x_t, .stp, .step file type if possible. Show More
ClCh_1720121
USB EZ-PD™ Type-C
Dear Sir, Our customer have a new project for Two Type-C port charge through power adapter with wireless charging as attached picture "ChargeThroughPo... Show More
SuSh_1535366
USB EZ-PD™ Type-C
  Hello, The HX3C data sheet contains the following information."If any particular section of the device function not required, then that sectionalone... Show More
JoLu_3455101
USB EZ-PD™ Type-C
Hi, The PMG1-S1 has an internal USB2.0 data mux (USBDP_TOP/USBDM_TOP and USBDP_BOT/USBDM_BOT). For our charger application, we do not need USB data. W... Show More
td83
USB EZ-PD™ Type-C
Hi, On our board we have 2 devices CYPD5225. Is it possible to link on the same SWD I2C bus the two devices ? I am using the "PSOC Programmer 3.29.1" ... Show More
td83
USB EZ-PD™ Type-C
Hi, On our board we are using the device CYPD5225 with a Tiger Lake. The Tiger Lake supports DP++ Display over Type-C ports. In DisplayPort mode the b... Show More
Board Information

USB EZ-PD™ Type-C

Discussion forum regarding USB EZ-PD™ Type-C topics.
Top liked authors