Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB EZ-PD™ Type-C Forum Discussions

Sort by:
Sophie_Wang
USB EZ-PD™ Type-C

Hi CY Friend,

如题。还是只能工作在DRP模式下?

谢谢

sophie

TeMa_2997106
USB EZ-PD™ Type-C
Configuration Utilityを用いて、Port Information→PR_Swap responseの項目をRejectからAcceptに変更しました。しかし、このConfigurationを適用したCCG3にてパケットを確認しますと、通信相手のデバイスからPR_Swapを送信され... Show More
DaSa_4627446
USB EZ-PD™ Type-C
Hello, We were settling on CCG3PA in a new design which is a Type C/Type A dual port charging only, with fixed 5V supply. I had a few more questions a... Show More
JoIs_3887151
USB EZ-PD™ Type-C
I want to build a system with USB Type-C (both UFP/DFP power ports) and need to select a CCGx device.I need to transfer 100W and have VBUS short prote... Show More
DaEr_349131
USB EZ-PD™ Type-C
Hi,There is an "old" reference design with CCG3PA + ACT475x. Question:- Is there source-code available for the Qorvo buck/boost available?- If yes, do... Show More
NoAr_1540581
USB EZ-PD™ Type-C
Hello They plan to write CCG5 Firmware  to CCG5C using Miniprog or ROM writer, but is it possible to program CCG5 build FW to CCG5C?Since the PartNumb... Show More
AdBi_4635021
USB EZ-PD™ Type-C
I am working on implementing my first USB PD design, and I have been having difficulties determining what the right controller IC for my product appli... Show More
MuIc_4620061
USB EZ-PD™ Type-C
Hi,I want to design a USB-PD application. I want to add PD functionality for a device that has no PD functionality. I also want to show voltage and cu... Show More
DaEr_349131
USB EZ-PD™ Type-C
Hi,For CCG5 or CCG6, what's the best/fastest way to flash the firmware onto the CCG's?Note: we have to run from Linux machines, so miniprog/psoc progr... Show More
TeMa_2997106
USB EZ-PD™ Type-C
現在CCG3に設定しているすべてのSource PDOに対し、EZ-PD Configration Utilityを用いて[Unchunked Extend Messages Supported]をYesからNoに設定変更しました。 しかしながら、このConfigurationを適用したCCG3にて... Show More