Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB EZ-PD™ Type-C Forum Discussions

Sort by:
JoLu_3455101
USB EZ-PD™ Type-C
Hi For a sink-only application using CCG3PA (CYPD3171), VBUS_IN is connected on the Type-C Receptacle side, but should VBUS_C_MON pin be connected to ... Show More
Jiong
USB EZ-PD™ Type-C
Hi team   As shown in the following figure, I use scb4 as i2C.How to choose the clock parameters on the right?   Thanks Jiong   Show More
kms
USB EZ-PD™ Type-C
Hi, infineon team.   I wanna ask something about CYPD3120-40LQXI DisplayPort example. If we don't have a DFP sink, can we change the [example Display ... Show More
ArthurHsu
USB EZ-PD™ Type-C
你好 在EZ-PD™ CCGx Power SDK裡的CCG3PA範例裡可以看到HPI相關的程式 把config.h裡 #define CCG_HPI_ENABLE設為1後,重新編譯會出現錯誤 請問這要怎麼處理 謝謝 Show More
Jiong
USB EZ-PD™ Type-C
Hi,team   When I create a custom PMG BSP in BSP Assistant 1.0, I found that there is no generic PMG BSP which can be used as a template in BSP Assista... Show More
BhargavGolla
USB EZ-PD™ Type-C
Hi , I am using CCG3PA as DRP ,  Setup: Connected 2 CCG3PA one as source and other sink,  1. From sink APDO 6 is been request 16v, min 3v3 and 3Amp 2.... Show More
KyleLin
USB EZ-PD™ Type-C

Hi,

If I use CY4500 to catch EPR 28V, will it be damaged by 28V?

Regards,

Kyle

eric_engineer
USB EZ-PD™ Type-C
How do I download the DOWNLOAD - EZ-PD™ Configuration Utility?  It seems to be "locked" on the website. I have an NDA with Cypress but I'm not sure ho... Show More
daver
USB EZ-PD™ Type-C
follow up to the issue  "CYPD3120 configuration for a USB-C display port alt mode sink" Hi Mohamed,   We looked at the suggestion, but I think there m... Show More
Danio_A
USB EZ-PD™ Type-C
CYPD 4226 UFP
solved msg Solved
Hello,Our design scheme is: through CYPD4226 chip to control tusb1064 to complete the transmission of video signals from PC to FPGA. Shall we switch t... Show More