- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
In CCGx Host SDK User Guide @ https://www.cypress.com/file/432036/download , I can follow Section 5.2, which runs through and shows the high level process flow.
There are three basic steps:
- Define the configuration:
- Reference Configuration Utility User Manual on how to create a .cyacd file. https://www.cypress.com/file/183686/download , “Note that the XML file itself cannot be programmed to the device. A special file with “cyacd” extension is saved along with the XML file to the selected folder. This file should be used to program the configuration to the device.”
- Define the firmware program desired:
Option 1: Use PSoC Creator to add any modifications to the base firmware for any device
- Reference “What is required for PSoC Creator 4.x to support CCG parts?” @ https://community.cypress.com/thread/53395
- Reference “CCG2 development environment - What is the process to setup?” @ https://community.cypress.com/message/204280
Option 2: Obtain the default firmware from Cypress
- Reference “CCG Bootloader Project Files” @ https://community.cypress.com/thread/53149
- Program the device
- **** Detailed instructions for this step are eluding me **** <<== What are the steps to merge the cyacd and hex files??
- Merge .cyacd Configuration file into .hex Firmware file
- Use PSoC Programmer to load into the device
Greg
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Greg,
Yes, the procedure is different for CCG2. Since you are importing the project from the CCGx SDK, please follow the procedure in Import EZ-PD Configuration Utility C-source on PSoC Creator 3.3.
Since the libraries for the CCGx SDK are pre-built to be supported on PSoC Creator 3.3, we recommend building the example projects on the same IDE version.
If the errors are same as mentioned in https://community.cypress.com/message/233686?et=watches.email.thread#233686 , please follow up on the same.
Best Regards,
Sananya