Announcements

Live Webinar: USB-C adoption. Simple & Cost-efficient solutions | April 18th @9am or 5pm CEST. Register now !

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi,

Need to understand how HPD IRQ bit status field will be used from DFP side application code to generate HPD signal.

Is this bit important to trigger the HPD signal? or just HPD status is enough.

Thank you,

0 Likes
3 Replies
ShifangZ_26
Moderator
Moderator
Moderator
10 likes given 250 sign-ins 1000 replies posted

Hi Arun,

HPD IRQ and HPD have defined timing and occurred condition in DisplayPort SPEC. For the signal HPD is HIGH or LOW, the DFP will generate HPD signal as per HPD's status. If HPD IRQ bit status is assert, DFP should follow DisplayPort SPEC generate IRQ plus on HPD signals.

Since you asking those information, I could like to say, if you found IRQ bit is assert, which is equal to the DispalyPort sink have detected DisplayPort source's signal but the signals can not show up on the screen.

Best Regards,

Lisa

0 Likes
Anonymous
Not applicable

Hi Lisa,

w.r.t customized design CCG3 CYPD3120 based dongle logic(UFP) is tightly coupled with display module(we can't do DP plug-in/out, DP lines are routed to DP Receiver pins directly). After USB-C plug-in we will power on this system.

Display module will provide HPD to CYPD-3120 always hope this should not cause problem. What I am expected is, when we plug USB-C to DFP device system will power on and in one of VDM mesage UFP will send attention command and followed by Status message about HPD, status. why UFP is not no able to set HPD IRQ bit.

CYPD 3120 will know HPD input on power on but, why its missing to capture the IRQ bit setting during power on? Will this timing can be modified at application level?

Thank you,    

0 Likes

Hi Arun,

Could you please share your cc log (captured by PD analyzer) and the scope with HPD signals to me? Since CCG3 C to DP firmware have realized IRQ and HPD and reflect to CC message. The two types message will carry HPD information -- DisplayPort Status Updates and Attention.

If IRQ have alreadt shows up, the bit[8] will show up the status.

Best Regards,

Lisa

0 Likes