Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB EZ-PD™ Type-C Forum Discussions

Yaodong
Level 3
Level 3
First solution authored 10 replies posted First like given

Hello.

I am developing Microdisplay with USB-C port (based on CCG3). The display should act as UFP and Sink, it can be powered and receive Display-data through the C-port of the laptop.

Is there a specific chip that acts only as UFP and Sink, or do I have to buy the DRP chip and then program or configure it?

Thanks a lot.

Yaodong

你好,

我正在开发有USB-C型接口的微型显示屏(基于CCG3)。显示屏应该作为UFP和Sink,它能通过笔记本电脑的C口接受供电和接受视频数据。

是否有一个特定的芯片只作为UFP和Sink,或者说我必须买DRP的芯片再对它进行编程或配置?

谢谢

Yaodong

0 Likes
1 Solution
ShifangZ_26
Moderator
Moderator
Moderator
10 likes given 250 sign-ins 1000 replies posted

Hello Yaodong,

可以直接选择CYPD3120,这颗芯片是由Infineon已经预先烧录好固件,并且对应的是UFP和Sink。当然,如果你想再进行配置,也是可以的。CYPD3120这颗芯片内置Billboard,并且提供USB bootloader,可以在使用Infineon的Ez-PD configuration Utility进行参数或者固件升级。

 

Best Regards,

Lisa

View solution in original post

0 Likes
4 Replies
HmdRahmathulla
Moderator
Moderator
Moderator
10 likes received 100 sign-ins 25 solutions authored

 Hi Yaodong,

Thank you for posting in infineon community.

Our CCG3 is user programmable according to the application needs. but we dont have specific IC for the application which you are looking.

you can configure the CCG3 chip as UFP and Sink role using Psoc creator or EZ-PD configuration utility.

we have also provided USB-C to DP sample program for the reference.

 

Thanks & Regards

Mohamed Rahmathulla

 

0 Likes
ShifangZ_26
Moderator
Moderator
Moderator
10 likes given 250 sign-ins 1000 replies posted

Hello Yaodong,

可以直接选择CYPD3120,这颗芯片是由Infineon已经预先烧录好固件,并且对应的是UFP和Sink。当然,如果你想再进行配置,也是可以的。CYPD3120这颗芯片内置Billboard,并且提供USB bootloader,可以在使用Infineon的Ez-PD configuration Utility进行参数或者固件升级。

 

Best Regards,

Lisa

0 Likes

你好 Lisa

谢谢你的回答。

我还有个问题,Billboard具体是什么,它有什么作用?

Best Regards,

Yaodong

0 Likes
ShifangZ_26
Moderator
Moderator
Moderator
10 likes given 250 sign-ins 1000 replies posted

Hello Yaodong,

Billboard 可以简单的看成Alternate Mode设备(UFP)的身份信息的USB2.0设备。Billboard的信息构架与USB2.0 设备基本一致,当Alternate Mode进入失败,Billboard一定需要被枚举,以便进行设备状态查询,reset,更新。

 

Best Regards,

Lisa

0 Likes