Dear all,
I'm thinking of a solution to add a Type-C to DisplayPort monitor.
That port needs the function to charge connected devices while receiving DisplayPort in alternate mode.
When I searched the reference design, I found a "Type-C-DisplayPort Cable" using CCG3.
But it was Sink, not PD Source.
Can I achieve this solution by making the following changes based on the "Type-C-DisplayPort Cable" and "Power Bank" reference designs?
-Port the Provider path of "Power Bank" to "Type-C to DisplayPort Cable".
-Replace CYPD3120 of "Type-C to DisplayPort Cable" to CYPD3121.
-Use the CCG3 Monitor Project of the EZ-PD Configuration Tool.
Best Regards,
Hidekazu Omoi
Solved! Go to Solution.
Hi,
Yes, the reference design chosen and steps mentioned are correct. Please refer to the blog post on this topic - https://community.cypress.com/t5/Resource-Library/CCG3-Type-C-receptacle-DRP-Reference-Design-Power-...
Hi,
Yes, the reference design chosen and steps mentioned are correct. Please refer to the blog post on this topic - https://community.cypress.com/t5/Resource-Library/CCG3-Type-C-receptacle-DRP-Reference-Design-Power-...