Two I2C buses in CCG3PA

Announcements

Live Webinar: USB-C adoption. Simple & Cost-efficient solutions | April 18th @9am or 5pm CEST. Register now !

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
cshin
Level 1
Level 1
First reply posted First like given First question asked

Hello,

Can I use two I2C buses simultaneously in a CCG3PA device? One is for host communication and the other is for an external DAC access.

The CCG3PA device has three I2C buses as

1. P0.0 I2C_0_SDA, P0.1 I2C_0_SCL
2. P1.0 I2C_1_SDA:1, P1.1 I2C_1_SCL:1
3. P2.2 I2C_1_SDA:0, P2.3 I2C_1_SCL:0

I'd like to use 2 and 3 together, want to doublecheck if it's okay because it has :1 and :0 suffixes.

Thanks,

Choon

0 Likes
1 Solution
HmdRahmathulla
Moderator
Moderator
Moderator
100 solutions authored 250 sign-ins 25 likes received

Hi Choon,

Thank you for creating post in infineon community.

 CCG3PA has only I2C buses. 

1. P0.0 I2C_0_SDA, P0.1 I2C_0_SCL  -->  it is fall in SWD program pins, it will affect your debug.

 ( P1.0 I2C_1_SDA:1, P1.1 I2C_1_SCL:1) & (P2.2 I2C_1_SDA:0, P2.3 I2C_1_SCL:0 ) you can use for your project together. 

you can refer section 1:3:1 in the below link.

https://www.infineon.com/dgdl/Infineon-EZ-PD(TM)_CCG3PA_Datasheet_USB_Type-C_Port_Controller-DataShe...

Thanks & Regards

Mohamed Rahmathulla

View solution in original post

2 Replies
HmdRahmathulla
Moderator
Moderator
Moderator
100 solutions authored 250 sign-ins 25 likes received

Hi Choon,

Thank you for creating post in infineon community.

 CCG3PA has only I2C buses. 

1. P0.0 I2C_0_SDA, P0.1 I2C_0_SCL  -->  it is fall in SWD program pins, it will affect your debug.

 ( P1.0 I2C_1_SDA:1, P1.1 I2C_1_SCL:1) & (P2.2 I2C_1_SDA:0, P2.3 I2C_1_SCL:0 ) you can use for your project together. 

you can refer section 1:3:1 in the below link.

https://www.infineon.com/dgdl/Infineon-EZ-PD(TM)_CCG3PA_Datasheet_USB_Type-C_Port_Controller-DataShe...

Thanks & Regards

Mohamed Rahmathulla

Thank you so much for confirmation!

0 Likes