- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Dear all,
First of, apologies if I've missed this as a FAQ, but haven't been able to find a similar query.
I'm looking into designing a multi-port rear seat charger with the CCG3PA. So far, I've not been able to find any design resources (such as datasheets and reference designs ...etc) on the Infineon website.
Am I missing something? is there a process to go through, in order to gain access?
Thanks in advance.

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi,
Thank you for posting on the Infineon Community.
At Infineon, we do have reference designs for rear seat charger using CCG3PA ( CYPD3196 ).
The different reference design kits and their comparison is as shown below,
For the automotive sdk support and reference designs, please contact local sales / FAE.
For latest designs it is recommended to use CCG7D Type C port controller with integrated buck boost controller. EZ-PD™ CCG7D is a highly integrated and programable dual-port USB Type-C Power Delivery (PD) solution with integrated Buck-Boost controllers. It complies to the latest USB Type-C and PD specifications, and is targeted for multi-port consumer charging applications. CCG7D supports a wide input voltage range (4V-24V with 40V tolerance) and programmable switching frequency (150 kHz-600 kHz) in an integrated PD solution. Integration offered by CCG7D not only reduces the BOM but also provides a footprint optimized solution to support higher power density designs. CCG7D supports advanced features such as dynamic load-sharing, signed field firmware upgrade, and optimized buck input voltage.
For datasheet, reference designs and demo boards, please contact Infineon local sales office / FAE.
I hope the above explanation has helped you in knowing the different rear seat charger controllers from Infineon.
Regards,
Abhilash P